Part Number: DRV2605 Other Parts Discussed in Thread: DRV8601 Tool/software: Hi team,
We have taken out the Out+, Out- signal from haptic connector, whether we need to connect some haptic device to get the data. The signal lines are connected to PMIC…
Part Number: DRV2605 Other Parts Discussed in Thread: , USB2ANY
Tool/software:
Hi Team
In document of SLOC283, I see 123 effects that drv2605 can play, are these 123 effects built in ROM of drv2605 or we need to flash to drv2605 by ourselves?
As of…
Hello Sydney, I don't see this issue any more after we pulled in latest driver changes for the RTOS we are using. Thank you for your support!!
Regards
Vijay
Part Number: DRV2605 On a project that has sold hundreds of units, we occasionally have an electrical board fail, with the symptom that the motor no longer vibrates.
We've carried out a number of investigations and have come to the conclusion that in…
Part Number: DRV2605 Hi Sir,
My customer is surveying the DRV2605, could it support driving the below HAPTIC Reactor Heavy device? Thanks!
product_spec_afr14a901b_zh_hans_49f862c1b8.pdf
Part Number: DRV2605 Other Parts Discussed in Thread: DRV2624 , Hi team,
Is DRV2605 a suitable solution to replace DW7912 or we have other product is more fit?
Regards,
Alex
Part Number: DRV2605 Hello
I have an application where I'd like to fix the LRM frequency at ~170Hz - no auto resonance desired.
Is this achievable by doing the following?
Set LRA_OPEN_LOOP bit to 1 in register 0x1D
Set N_ERM_LRA bit to 1 in register…
Part Number: DRV2605 Other Parts Discussed in Thread: USB2ANY , , Dear Sir or Madame,
Let me introduce myself, my name is Abel Fontserè and I am working as electronics engineer at CERO design, Barcelona.
Currently, I am working in haptic feedback…
Part Number: DRV2605 Hi there
I am looking at using the DRV2605 Haptic Driver to drive an ERM motor in an upcoming project. The ERM motor has an operating voltage between 2.7V and 5V and has a rated current of 60 mA.
I am unable to find any information…