Part Number: DRV2605
(My customer support ticketed asked that I post to the form to get answers.)
We are planning on having 4 DRV2605YZFR parts on the same I2C bus. Our plan is to wire the EN pins of each Haptic Driver to separate GPIOs of the MCU. However…
Part Number: DRV2605 Other Parts Discussed in Thread: DRV2604 Hi team,
2 Quick questions surrounding DRV2605:
The DRV2605 device offers a licensed version of the TouchSense 2200 software from Immersion. Can we use it without Immersion library?
If so…
Part Number: DRV2605 Hi we choose the TI haptic motor drive DRV2605 for a ERM vibrator, SMD type, my question is :
on the same PCB layer (the bottom one) we have some traces running into the area under the rotating mass: may this give us any troubleshootings…
Other Parts Discussed in Thread: DRV2605L Hi we choose the TI haptic motor drive DRV2605L for a ERM vibrator, SMD type, my question is :
on the same PCB layer (the bottom one) we have some traces running into the area under the rotating mass: may this…
Part Number: DRV2605 May I ask whether the settings of the registers 0x16, 0x17, 0x1A are mainly determined the last settings, or is it recommended to determined in the Auto-Calibration stage?
1. Will the settings set in the Initialization stage be overwritten…
Part Number: DRV2605
For the LRA clamp voltage, the equation(7) do not match the "Table 8. LRA Auto-Calibration Example" of "DRV2605 setup guide".
In the setup guide, the HEX value is A0, setting clamp voltage is 2.82V.
Via the equation…
Part Number: DRV2605EVM-CT Other Parts Discussed in Thread: DRV2605 I want to remotely control the vibration of DRV2605 through the computer, instead of touching B1 and B2 to trigger the vibration. I want to know whether this product supports it, and if…
Hello,
Is any limitation or rule to the ERM vibrator when I choose a new one for drv2605?
Key specification to the vibrator:
(1) Operating voltage: DC 2.0 V
(2) Operating voltage range: 1.5– 2.5V
(3) Terminal resistance: 33.0±3.0Ω…