Part Number: DRV2605L Other Parts Discussed in Thread: DRV2605 Hi:
I have a question about the LRA Initialization example in <DRV2605 Setup Guide> as below:
What should I set to register 0x18 and 0x19? Could I use the default value without setting…
Part Number: DRV2605L Other Parts Discussed in Thread: TCA9548A , I have one question about using this motor driver.
I connected three DRVs to TCA9548A (Multiplexer).
First DRV is connected to SD0/SC0, second one is connected to SD1/SC1, and last…
Part Number: DRV2605L Other Parts Discussed in Thread: DRV2605 When I saw the datasheet about Waveform sequencer,
it described that when I set the bit 7 (Wait bit) for Waveform Sequencer, WAV_FRM_SEQ[6:0] bit will be interpreted as a wait time. It means…
Part Number: DRV2605L Tool/software: I am working on a project utilizing the DRV2605L and would like to drive the IN/TRIG pin with and audio signal that is 400mV p-p.
If I understand correctly, the data sheet documentation describes a method to modify…
Part Number: DRV2605L-Q1 Hi,
The customer wants to add a haptic function to the column SBW.
Is it possible to diagnose the OPEN SHORT status of the actuator only when it is active?
Part Number: DRV2605L-Q1 Other Parts Discussed in Thread: DRV2605L Dear TI engineer
This is Johnson.
Here are the questions about DRV2605-Q1
(1) If DRV2605-Q1 support Real time playback, what's the input frequency in I2C? And what tools I can use…
Part Number: DRV2605L Hi All,
I have a question about DRV2605L.
Is f(LRA) in equation (5) in 8.5.2.1 Rated Voltage Programming the desired frequency to drive the actuator within 125-300Hz?
Best Regards, Ishiwata
Part Number: DRV2605L Hi,
I am using the DRV2605L to design a prototype for a haptics based product. I am having issues getting the autocalibration to complete successfully. I am using an LRA in closed loop mode. The LRA has the following parameters…
Part Number: DRV2605L-Q1 Other Parts Discussed in Thread: DRV2605L Hi team,
Customer connect VDD to EN pins. When customer pull up SCL and SDA with 5V and VDD/EN don't have 5V input, customer found that there is around 5V at VDD/EN pin. Is that reasonable…
Part Number: DRV2605L Other Parts Discussed in Thread: DRV2605 Dear experts In our project we are using the DRV2605L in combination with an LRA (240Hz resonance, 0.1...1.2Vrms drive voltage). The DRV2605 is in closed loop mode with PWM input (f=20kHz…