Hi Ricardo,
I just spoke with a colleague, and you can follow the instructions in the DRV2605LEVM-CT user guide, section 6. The first bullet point in section 1 has an alternative method for programming using a MSP430 LaunchPad.
I'm sorry that we have…
Part Number: DRV2605L Other Parts Discussed in Thread: USB2ANY , , EV2400 hello
I am using DRV2605L, and I want to know the methods to enhance the strength of vibration.
and i want to perform DRV2605LEVM-CT through Haptic Control Console GUI, but i don't…
Actually I need to clarify, this is a DRV2605LEVM-CT. Seems like the newest firmware is sept 2014
www.ti.com/.../DRV2605LEVM-CT
So Im not thinking I could be much behind.
Apparently I need an msp430 to update anyway which I dont have on me. Is there…
Hi, Blake:
www.ti.com/.../drv2605levm-ct
on the page of above link, you can find the firmware for DRV2605LEVM-CT, "DRV2605LEVM-CT Firmware"
there are some code on how to program this device.
Thanks.
Hi Sasa,
No worries.
I want to suggest debugging with the DRV2605LEVM-CT + USB2ANY through Haptic Control Console. Do you have these boards? We were previously using the DRV-USBCOM-EVM for communication, but we switched to the USB2ANY.
Other Parts Discussed in Thread: DRV2605LEVM-CT , DRV2603 , DRV2605L , DRV2625 , DRV2605 , MSP430TCH5E I did not see the HapTouch_GUI - PC tool to drive haptics and create new haptics sequences, and program them to the BoosterPack included in the SDK.
I am…
Other Parts Discussed in Thread: DRV2605L , DRV2605LEVM-CT Is it Possible to drive the LRA motor continuously using this DRV2605L break board and connecting it with Arduino? If yes what pins should I use.Thanks
Other Parts Discussed in Thread: DRV2605LEVM-MD , DRV2605LEVM-CT , MSP430F5510 , DRV2605L Hi,
I'm currently trying to customize the DRV2605LEVM-MD firmware to set how many motors and which type are connected, following section 3.4 in the manual. The thing…
Hi, Craig:
which EVM are you using? (DRV2605LEVM-CT? DRV2605L miniEVM?)
if yes, do you have the DRV-USB-COM board?
if you have the COM board and one of our EVM, we can walk through how to use Haptic Control Console for DRV2605L.
Thanks.
Nabeel,
Since this was a long ago, I will try and look for it. I would recommend that you take a look at the MSP430 library. (Almost all the files you would need could be imported from this firmware)
www.ti.com/.../drv2605levm-ct Documents
Regards,
…