Part Number: DRV2625 Hello,
I have a LRA motor with the these specification:
Frequency: 100Hz
Resistance: 6.5E
Rated current: 300mArms
Rated voltage: 2Vrms
According to the datasheet, the drive time should be 5msec. But the maximum drive time…
Part Number: DRV2605 Other Parts Discussed in Thread: DRV2625 Hello.
I have a question about the difference between DRV2625 and DRV2605. I would like to output the waveform of the internal library to the LRA device in open loop using I2C.
Is there…
Part Number: DRV2625
Hello,
My customer is trying to figure out how to handle the calibration routine for the DRV2625 for production and is looking for some feedback.
Could they characterize a number of LRAs and program the average calibration…
Part Number: DRV2625 Hi team,
What is the calculation between voltage and the register value for BAT_LIFE_EXT (0x0A and 0x0B). I am not finding anything in the datasheet or excel calculator.
Thanks,
Ben
Part Number: DRV2625 Dear Sir/Ms.
My customer designed DRV2625 on their wearable device, and it is now in trial production. One question they have is that DRV2625 needs to be calibrated during production?
Currently my customer application is used…
Part Number: DRV2625 Other Parts Discussed in Thread: DRV2605 , , DRV2605L Hi Team,
The customer is going to replace DRV2625 with DRV2605. They compared the register sets between DRV2625 and DRV2605, the below register and feature are used in DRV2625…
Part Number: DRV2625 Hi Team, The datasheet shows the following. ----------------------------- (page 27) 8.6.7 Calibration Routine The DRV2625 has a calibration routine that automatically populates all critical parameters required for successfully driving…
Part Number: DRV2625 Different document number of Package outline of DRV2625
Datasheet - YFF009-C01 doc. 4221850/A 01/2015 (see page 70-72) www.ti.com/.../drv2625.pdf
Package Outline link in website - YFF0009 doc.4219552/A 05/2016 www.ti.com/…
Part Number: DRV2625 Hi Team, My customer considers to use DRV2625 with LRA for small hand-held electronic application. The application is assumed to vibrate while holding in one hand. If so, I believe DRV2625 auto calibration should be applied under…