Part Number: DRV2625 Other Parts Discussed in Thread: DRV2605L , Hi Team,
I would like to know the current consumption when active.
In DRV2605L, I(BAT_AV) is mentioned.
Please let me know the value under similar conditions.
Best Regards,
Kenji
Part Number: DRV2625 Other Parts Discussed in Thread: TCA9548A , TCA9554 The DRV262x and DRV260x devices has a TI haptic broadcast mode where it will make the device respond to the slave address 0x58 (7-bit) or 1011000 in binary. This mode is useful in…
Hello,
The 0x2D register is unused. There is nothing you need to do with it.
The 0x2B are spare bits in the DRV2625. The ECO mode noted in the Control Console is actually a hold over from another device.
Best Regards,
Justin Beigel
Part Number: DRV2625
Hi,
I cannot find anywhere any specific information about individual effects in the waveform library. Could you share that with me?
Thanks,
Marta
Part Number: DRV2625 Hi
Now we use I2C to control DRV2625 and set TRIG/INTZ to low
If we set TRIG/INTZ to high, anything happen? Or any register value will change?
Thank you~~
Poki
Part Number: DRV2625EVM-MINI Other Parts Discussed in Thread: BQ25611D , DRV2625 , Tool/software: Hi Ti, We are using the following battery gauging module BQ27421-G1B EVM along with a charger module BQ25611d EVM , and it’s all interfaced with ARM processor…
Part Number: DRV2625 Hi team,
Customer is using DRV2625 to drive ERM motor. setting closed-loop, RATED_VOLTAGE[7:0]=0X89 (expect 3V), however the EVM output 2.8V and customer board output 3.5V with the same setting.
Do you know what else registers could…
Part Number: DRV2625 Hi Team,
Are there any mechanical requirements to achieve optimal DRV2625 auto-calibration results? If so, do we have any recommendations on placement or securing of the device while performing production auto-calibration?
Thanks…
Part Number: DRV2625 Hi TI:
Do D RV2625 have any Errata document might impact HW design?
If yes, please provide Errata document
And please help check attached our EVT stage DRV2625 SCH and layout ok or not based on latest datasheet and Errata document
Thank…
Part Number: DRV2625 1. I want to know whether W0525AB001D ERM Actuator is compatible with DRV2625. The datasheet doesn't have a detailed recommendation on the compatible ERM actuator parameters. 2. I'll interfacing DRV2625 with NRF52 through I2C…