Part Number: DRV2625EVM-CT Do any of the haptic motor eval kits have support for Windows 11? When I attempted to use the DRV2625EVM-CT, the Haptic Control Console 1.6.0.2 crashes when I press 'connect'. I see from a different forum post that I would need…
Part Number: DRV2625EVM-CT I marked my previous question as closed too soon, the program still crashes 90% of the time when I try connecting the the Haptic Control Console to the DRV2625EVM-CT.
Do any of the other haptic motor eval kits have support for…
Part Number: DRV2625EVM-CT Other Parts Discussed in Thread: DRV2625EVM-MINI , DRV2625 Hello,
I am using the DRV2525EVM-CT to evaluate an external LRA device. I would like to set the LRA device inside the enclosure and evaluate it using I2C communication…
Part Number: DRV2625EVM-CT Hello team,
Where can I find iOS apps to control DRV2625EVM-CT via Bluetooth, which is written in 3.2 Accessing Bluetooth Mode of user's guide?
Best regards,
Hideki
Part Number: DRV2625EVM-CT Other Parts Discussed in Thread: DRV2625 , MSP-FET , Hi,
I want to reprogram to create new haptic effects on the DRV2625 EVM-CT.
Therefore, based on the User's guide, I purchased MSP-FET MCU Programmer and Debugger for reprogramming…
Part Number: DRV2625EVM-CT Other Parts Discussed in Thread: DRV2625 , As the title suggests, we would like to know what is the supported range and resolution of Gs (ERM)? For example: Are we able to go from 0 to 1/2 Gs, in 0.01 increments?
Part Number: DRV2625EVM-CT In waveform sequence, I choose 47Buzz1-100%,what is the time of 47 Buzz1-100%?
What is the time in ms for waveform 47 to run once?
If I want to set up the 47Buzz1-100% run 1s then stop 1s, how to set?
BR,
Gust
Part Number: DRV2625EVM-CT Hi Team,
As the below figure shows, when I press 'Connect' to access the device Console, the GUI will stop working. My OS version is windows 10 pro. Could you tell me how to solve this issues? Thanks!
Part Number: DRV2625EVM-CT Other Parts Discussed in Thread: USB2ANY , , DRV2625 Is there any way to work with this board in Windows 10?
Kind regards,
Jorge Elizalde
Part Number: DRV2624EVM-CT Other Parts Discussed in Thread: DRV2625EVM-CT , Hi
Is there any HCC update information for DRV2624EVM-CT and DRV2625EVM-CT for Windows 10?
Support for Windows 7 will soon be over.
Thank you!