Part Number: DRV2700EVM-HV500 Hello,
In the DRV2700EVM-HV500 you have choosen the mosfet BSS127 H6327XTSA2, could you please suggest to me an appropriate mosfet for a 800V application (I_out= 10mA).
Thank you for your support.
Part Number: DRV2700EVM-HV500 Other Parts Discussed in Thread: DRV2700 Tool/software: I have accidentally provided 12V to DRV2700EVM-HV500. There is no output from the board. I have seen that there is a Zener diode D2 SOD-123 MMSZ5232B-7-F placed on the…
Part Number: DRV2700EVM-HV500 Tool/software: Hello Sydney,
The 3D file that you provided to Mark Kruskopf (my colleague) does not match the items that we have.
Is there another file that we can try?
Thanks,
Aaron
Part Number: DRV2700EVM-HV500 Tool/software: Hi,
I'm trying to run the piezo load of 4.5nf using DRV2700EVM-HV500 evaluation board, the output is almost DC wave as shown below never the desired signal
Requesting support on how to resolve this
Piezo…
Part Number: DRV2700EVM-HV500 Hello,
I have a DRV2700EVM-HV500 and connected it using an external DC voltage signal as specified in the manual, with no load attached.
However, the output waveform (shown below) appears very noisy, although the input…
Part Number: DRV2700EVM-HV500 Other Parts Discussed in Thread: DRV2700 Hi Experts,
I am trying to drive piezos at voltages of about 100V pk-pk with frequencies above 20kHz. The data sheet for the DRV2700EVM-HV500 says the first Vmax is 158V. Can I connect…
Part Number: DRV2700EVM-HV500 Other Parts Discussed in Thread: DRV2700 I am driving a piezo actuator HD-PAF1419 on 212 using DRV2700EVM-HV500. I wan to know what maximum current amplifier can produce whike operating on 212V. According to graph between…
Part Number: DRV2700EVM Tool/software: How do I determine the maximum drive frequency of TI Piezo HV driver evaluation boards such as the DRV2700EVM or DRV2667EVM (or other) for a given piezo capacitance load? We need to specifically explore generating…