Jeong,
We just switched to a new system for managing secure files, could you navigate to https://www.ti.com/product/DRV3245Q-Q1 and click the request button shown?
Regards,
-Adam
Part Number: DRV3245Q-Q1 Hi, Team,
My customer found DRV3245 sometime will trig the STP_FAULT and DEADT_FAULT in their system, when the MCU's PWM with 1.5us deadtime(Setting by MCU). After checking the register setting, they found the 0x07 set as followed…
Part Number: DRV3245Q-Q1 Other Parts Discussed in Thread: DRV8316 , DRV8316-Q1
Hi Team,
The customer is reviewing DRV3245Q-Q1 for the joystick steering project.
* Delete blocks.
If you have a better BLDC driver for the project, please recommend it.
Part Number: DRV3245Q-Q1 Hi,
we are exploring the 1pwm method for DRV3245Q-Q1 Motor Driver.nfault pin is outputting high and when commutation is applied nfault is being pulled low.
We read SPI registers(ICStatus0,ov/vds,VGS,ICStatus1,ICStaus2) and there…
Part Number: DRV3245Q-Q1 Hi team,
My customer is consider using DRV3245-q1 in a transmission project. Customer would like to know under fault condition, could we configure in someway so that the duty cycle is a fixed value rather than directly shut down…
Part Number: DRV3245Q-Q1 The device has the CRC-8 check by using the polynomial X 8 + X 5 + X 3 + X 2 + X 1 + 1 .Currently we don’t have the CRC algorithm for this polynomial.
Could you please provide the sample code/algorithm for calculating CRC-8 with…
Part Number: DRV3245Q-Q1 I need help clarifying how the phase comparators work on the DRV3245 driver.
What does it mean, Each comparator is switching at 75% and 25%, or 50% of the VDRAIN voltage ?
The push-pull outputs are integral to the DRV3245 phase…
Part Number: DRV3245Q-Q1
Hello,
I would like to know more about the C-model. It seems that it basically completes any missing feature from both the existing models (by an additional current amplifier to the A and an additional phase comparator to the…