Part Number: DRV3255-Q1 Hi team,
I would like to know how to understand the 75% for rising and 25 for falling of PHC_TH. Why do we set 75% and 25% as options?
Thanks.
Part Number: DRV3255-Q1 Other Parts Discussed in Thread: C2000WARE Hi,
We are trying to flash the DRV325x_EVM_Basic_Trap_Comm code in the EVM using CCS v8.
Initially it was showing
Product"C2000ware_software_package v2.1.0.00 is not currently installed…
Part Number: DRV3255-Q1 Other Parts Discussed in Thread: TPA3255 Hi team,
The TPA3255Q1IC height is 1.0 to 1.2 mm on the spec sheet, and the height of the heat sink lock amplifier IC used for the demo board is 1.0 mm.
The customer would like to confirm…
Part Number: DRV3255-Q1 Hello
I am looking to use the DRV3255 on a new project. I know the part is not yet in production however I will need the commercial details with regards to:
When will the first full production devices be available?
What are the…
Part Number: DRV8353 Other Parts Discussed in Thread: DRV3255-Q1 Tool/software: I would like to request sch review of DRV8353. Can you please get back to me? Thx!
Part Number: DRV3255-Q1 My customer would like clarification on the following: Is the gate drive current controlled or do the different IDRIVE settings just change the source/sink resistance? It's a little unclear because of the inclusion of both current…
Part Number: DRV3256-Q1 Other Parts Discussed in Thread: DRV3255-Q1 , Tool/software: Can you please provide full ds to DRV3256-Q1 and DRV3255-Q1 ?
What are the critical differences?
Hello Likhith,
Thank you for your questions and interest. The closest reference design that we have for automotive 48V systems is TIDM-02017 reference design: https://www.ti.com/tool/TIDM-02017 . This design is rated for 5kW and used for the control of…
Hello, Make sure D1 is properly rated. Our Evaluation board showcases this one. Diode, Schottky, 30V, 0.2A, SOD-323 What is the Operation Status A reported from the gauge about the CHG bit? Is XCHG ever high? If XHG sets, this implies the FW wants the CHG…