Part Number: DRV3946-Q1 Other Parts Discussed in Thread: , DRV110 , DRV120 I am trying to use your DRV3946-q1 dual channel solenoid driver for a new design I am working on. I just got the approval to download the full data sheet.
I noticed that this…
Part Number: DRV3946-Q1 Tool/software:
Hi team,
I am looking for a design solution for one of automotive project (ABS). My requirement is a solenoid input voltage of 12V and a peak solenoid load current of 2A. Could you please suggest any suitable…
Part Number: DRV3946-Q1 Tool/software: Hello expert
An issue occur about the SPI Error Indicators and the LSD initiation failed.
I am doubting that the nFAULT/NAD pin Pull-up Resistor exceed the limit range.
One LSD's NAD pin pull-up Resister is…
Part Number: DRV3946-Q1 Tool/software: Hello, I am working on two DRV3946-Q1(5K NAD 00 and 12K NAD 01) IC with microcontroller TC377TP.
We had working project with single DRV3946 (12k – NAD 01) and same microcontroller and we were using it as base of…
Part Number: DRV3946-Q1 Tool/software: I wanted to integrate RTD with DRV3946 middleware driver so that we can create some application.
Please let me know if we already have such drivers compliant to ASIL B
Part Number: DRV3946-Q1 Tool/software: Good day, colleagues,
My customer has a question about the DRV3946 Command Register B0 to B4:
I want to vary the center frequency (to 20kHz with dither). But when I change the values, I always get the default…
Part Number: DRV3946-Q1 Tool/software: Hi team,
my customer use DRV3946-Q1 in BMS for BMW, they are doing IC Strip-line test, BMW require pass class 6 at 70-120M frequency. They are facing challenge to meet requirement.
I check the EMC report BU test…
Part Number: DRV3946-Q1 Tool/software: Hi experts
We use DRV3946 to drive relays with frequency of 20KHz, slew rate of 0x40, CE3 exceeded at 8M with P5 wire of relay control(HV+,HV-,DC+,DC- closed). The block as below. Detailed schematic attached too…