Ok, I think that I've got a wrong idea about SEL pin. 50ms is too much. What if we tie SEL pin low to ground and then apply a 50% duty-cycle 1000Hz signal to power input of DRV5012? Could be there any caveats if we are to control sampling frequency…
Part Number: TMAG5110 Other Parts Discussed in Thread: DRV5012 , , TMAG5111 Traditional window blinds are used to shade buildings by blocking the light coming through the windows. By placing a barrier between the window and the rest of the building, it…
Part Number: DRV5011 Other Parts Discussed in Thread: DRV5012 , Hi ,
we want to buy DRV5011ADDMRT but it is showing out of stock and high lead time , is there any alternate available for this with same configuration.
Regards,
Sayali
Sayali,
Unfortunately, the only Hall Effect latches we currently offer in the X2SON package are DRV5011 and DRV5012.
DRV5013, TMAG5110, and TMAG5111 are all capable of operating up to 38V, but these devices are all offered in either SOT23 or TO92.
Thank…
Part Number: DRV5032 Other Parts Discussed in Thread: DRV5012 We would like to use Digital-Switch Hall Effect Sensors in our RFID readers as tamper protection.
RFID means freq band HF (13.56MHz) and LF (125kHz) together. We need have to investigate both…
Part Number: DRV5032 Other Parts Discussed in Thread: DRV5012 , DRV5015 , DRV5013 , DRV5011 Hi Sir
May I know DRV5032 can do Incremental Rotary Encoding application ?
I saw DRV5012 have this application ,but not sure DRV5032 can do as well
Thanks
Part Number: DRV5032 Other Parts Discussed in Thread: DRV5012 Hi
I am looking for ultra low power bipolar hall sensor. I found that DRV5032 is low power device. can some please explain me in details what will be the power consumption when there is no…
Part Number: DRV5011 Other Parts Discussed in Thread: DRV5032 , DRV5012 Hi Team,
There is a product requirement as follows:
Closed product structure, powered by coin-cell battery
Long-term storage (more than 1 year) after production is completed
When…
Hi David,
No the DRV5012 would require lateral movement of the magnet as shown in my last post. You will likely need a magnet with thickness <<1.5mm to change the output state of the DRV5012 over the 1.5mm travel.
For the orientation you have…