Part Number: DRV5015 Other Parts Discussed in Thread: DRV425 Hi Team,
My customer is looking for a omni-polar hall effect sensor with very high sensitivity (the magnet disc they use is with 2.8mT at 20mm distance.) Could only find DRV5015 with such sensitivity…
Part Number: DRV5015 Other Parts Discussed in Thread: DRV5032 , DRV5012 , DRV425 Hi Team,
My customer was searching for a hall sensor which has similar magnetic threshold pint(Bop =0.7mT) with DRV5015A1, but lower Icc. DRV5105A1 has 2mA Icc, it is too big…
Part Number: DRV5015-Q1 Dear Technical Support Team,
Do you have a solution to automotive shifters with hall sensor(DRV5xxx)?
If you have application example, please let me know.
Thanks,
Best regards,
Lawrence.
Part Number: DRV5015-Q1 Dear Sir/Madam,
I am desinging a test setup for a new shift drum in a geardbox. I need to be able to measure the angular position of the drum (360 degrees), this has to be done with an off-axis set up because a lack of space for…
Part Number: DRV5015 Hi Engineer,
Currently 128-pole logarithmic magnetic ring for magnetic ring, magnetic force 60m, distance less than 1mm;
The output signal is particularly large, and the position detection accuracy is only about 1 degree.
As can be…
Part Number: DRV5015-Q1 Other Parts Discussed in Thread: DRV5015 Hi Engineer,
Bob/Brp/Bhys parameters of DRV5015A1, how to calculate the detection accuracy corresponding to the chip? If we want to customize the magnet that matches this chip, can 128-pole…
Part Number: DRV5013-Q1 Other Parts Discussed in Thread: DRV5015-Q1 , DRV5023
Hi team,
Could you tell me this Hall element position and its tolerance for the simulation?
I need the values as below image shows at least.
I need this package height as well…
Other Parts Discussed in Thread: DRV5015-Q1 , DRV5013-Q1 , DRV5013 , DRV5011 Hello Team,
Please suggest latch type hall sensor which withstand lower temperature rating upto -55C. Package is not concern yet. Below are details of hall sensor specificatio…
Other Parts Discussed in Thread: DRV5013 , DRV5015 , DRV5055 Dear TI forum family,
We are now developing a new PMSM of higher power rating (>25kW).
Please suggest an SMD type of Hall Effect Sensor for position estimation. Please also help me to design…