Part Number: DRV5055 Hi,
We use DRV5055A3QDBZR for the motor speed encoder and 2pcs per board, and now, we find the waveform are different for this 2pcs, can you help to check our schematic and waveform to advise if there are any error or some solution…
Part Number: DRV5055 Hi,
Customer need us to provide the FMEDA of DRV5055A2QLPGM, DRV5055A1QLPGM, can you help to send to my email: liang.zhang@arrow.com , thanks.
Part Number: DRV5055 1. Packaging: 3 pins, TO-92 or TO-92S or similar packaging. Pin order as follows:
2. Pin length: ≥12.5mm
3. Power Supply Voltage: Supports both 3.3V and 5.0V
4. Power consumption: ≤3.5mA @ no load
5. Measurement range…
Part Number: DRV5055 Hello, We are working on a design utilizing DRV5055A1QDBZ. We are looking at optimizing the current of the design. During investigation we found the hall to be drawing ~6mA. This is out of range according to datasheet Rev C. I found…
Part Number: DRV5055 I have a design where it is desirable to use a 3.0V supply. This is the minimum supply voltage for the DRV5055, and my regulated 3.0V supply will operate in the range 2.95 - 3.05V, slightly below the DRV5055 minimum at times.
My…
Part Number: DRV5055-Q1 Other Parts Discussed in Thread: DRV5055 Tool/software: What are the functional differences between these 2 hall-effect sensors? Are they functionally equivalent?
DRV5055-Q1 ( DRV5055A3EDBZRQ1 )
DRV5055 ( DRV5055A3QDBZT …
Part Number: DRV5055 Currently using DRV5055A1QLPGM A better solution would be a unipolar version. Which TI part is a drop in replacement that is unipolar?