Part Number: DRV5055-Q1 Hi,
We are trying to use Hall sensor(DRV5055A1ELPGMQ1) for measuring the magnetic field intensity of a electromagnetic (12V KK-P20/15).
Can anyone help how to place hall sensor.
As per data sheet hall sensor output voltage should…
Part Number: DRV5055 Hi team,
Is there any introduction material for SNR measurement for hall IC?
Should we put a termination or buffer at the output when we measure the SNR of DRV5055?
Regards,
Thank You Scott Bryson,
1. Actually I am looking for DRV5055 sensor placement, like below image
So the size of magnet should be such that the flux are within 168mT at < 0.5mm distance.
Same criteria we can assume material as N42 & SmCo24 with inner…
Part Number: DRV5055-Q1 Hi team,
Hope you are doing good.
Do we have any recomended pcb layout for this sensor? If there is any can you share the details with us.
Regards
Vivek Gandham.
Part Number: DRV5055 Other Parts Discussed in Thread: MCT8316Z , , TMAG5173-Q1 , TMAG5170 , TMAG5273 , TMAG5115 Hi Dear,
1.Our customer's application is UAV pan-tilt control. At present, MCT8316Z with control algorithm has been selected, and external Hall…
Part Number: DRV5055
Hi, everybody. I have a question for you
I'm using the DRV5055 Hall sensor to distribute 90° for position reading.
Could you explain the fifth and sixth principles in more detail?
Part Number: DRV5055 Other Parts Discussed in Thread: DRV5032 , TMAG6181-Q1 Hi,
We are looking into using the DRV5055 analog Hall sensor for a position sensing application in a battery-powered device. To reduce the power consumption of the sensor, I am…
Part Number: DRV5055-5057EVM Other Parts Discussed in Thread: DRV5056 , , DRV5057 , DRV5055 Hi,
Good Day.
I thought the DRV5056 linear hall sensor should be a suitable starting point and bought the EVM for the same.
I would like to know that If I connect…
Part Number: DRV5055 I want to design a 0-500A current sensor with this IC. Our sensor core can produce 140mT @500A and with the 12.5mV/mT sensitivity option, I can get a bipolar sensing range of 0.7-4.2V. I am currently using A1365 from allegro and would…