Part Number: DRV5055-Q1 Tool/software: Hello, I'm working on a WCCA for the DRV5055A3-Q1 and trying to understand the variation on sensitivity vs supply voltage. The electrical characteristics table puts the sensitivity at 25mV/mT at 5.0V and Figure 5…
Part Number: DRV5055-Q1 Tool/software:
I use TIMSS to simulate two DRV5055. How can I view the simulation results of two sensors at the same time in one chart? Thank you.
Part Number: DRV5055-Q1 Hello.
I'm planning on using DRV5055A4QLPGM in one of my designs (for current sensing) and I cant seem to find information in the datasheet regarding the slew rate of the device.
Am I'm missing something? could you please direct…
Part Number: DRV5055-Q1 Other Parts Discussed in Thread: DRV5055 So, I need to simulate sensor the part number is, DRV5055 which linear hall effect sensor. which tool can I used to simulate the sensor.
Part Number: DRV5055-Q1 Other Parts Discussed in Thread: DRV5055 DRV5055A2ELPGQ is AEC-Q100 Grade 0. I would like to ask the question below :
Is this PEM (PLASTIC ENCAPSULATED MICROCIRCUITS) part?
What condition that TI use for HTRB or HTOL (High…
Part Number: DRV5055-Q1 Other Parts Discussed in Thread: DRV5055 , TMAG5170
Is DRV5055 capable of sensing changing magnetic field at 10000rpm motor speed, if the magnetic field is within the sensor limit?
The sensor is linear in nature, whereas its…
Part Number: DRV5055-Q1 Hi,
We are trying to use Hall sensor(DRV5055A1ELPGMQ1) for measuring the magnetic field intensity of a electromagnetic (12V KK-P20/15).
Can anyone help how to place hall sensor.
As per data sheet hall sensor output voltage…
Part Number: DRV5055-Q1 Hi team,
Hope you are doing good.
Do we have any recomended pcb layout for this sensor? If there is any can you share the details with us.
Regards
Vivek Gandham.
Part Number: DRV5055-Q1 Have a few questions in regards to a TI calculator I am using, Magnetic Sensing Proximity Tool. When I change the type of magnet from block to cylinder the data gets weird, is that correct?
Kavuri,
DRV5055-Q1 is typically used for detection of permanent magnets. However, it may be capable of what you are asking. As long as sufficient magnetic field is produced by your wire, the sensor should detect it. You must be very careful about sensor…