Part Number: DRV5056-Q1 Other Parts Discussed in Thread: DRV5056 Hi team,
I have two questions would like to check with you.
1. Referring to below formula, the Vout in equation 1 stands for the device's output, correct? Or we should use this equation…
Part Number: DRV5056-Q1 Hi Expert,
My customer is using DRV5056-Q1 is their new project. Have some questions for the calculation tools on ti.com.
There are 3 different calculation tools for DRV5056-Q1. Customer would like to use it to calculate the…
Part Number: DRV5056-Q1 Hi,
The TI tool takes into consideration d1 distance from the surface of the sensor IC for sensing of distance measurement.
Whereas, the sensing element is placed at 0.47mm inside the IC from the surface.
Do we need to take…
Part Number: DRV5056-Q1 Hi,
I'm developing a position detection system to control the position of a shaft as it slides past the hall sensor (see my picture below).
Due to space constraints, the magnet is fitted to the shaft.
The air gap between…
Part Number: DRV5056-Q1 Other Parts Discussed in Thread: DRV5056 Hi, I would like to know will the sensor transmit constant output while the magnet is rotating at d1 and d2 distance? (as shown in below figure) Will there be any added error in output voltage…
Part Number: DRV5056 Other Parts Discussed in Thread: DRV5055 Hello,
I am a bit confused on how the sensitivities and measurement ranges work for the DRV5056 and the DRV5055. I have 3 different hall-effect sensors (DRV5055 A3, DRV5055 A4, and the DRV5056…
Part Number: DRV5056 Other Parts Discussed in Thread: TMAG5273 Tool/software: Hello!
I have a design using multiple DRV5056-A3 hall effect sensor in the SOT-23 package. There is a magnet on the other side of the PCB moving perpendicular to the PCB…
Part Number: DRV5056-Q1 Other Parts Discussed in Thread: TMAG5110 , TMAG5111 , TMAG5110-5111EVM , DRV5055 , TMAG5170 , TMAG5273 , DRV5032
I need help in choosing a hall effect sensor. The application is to detect the revolution and direction of the…
Part Number: DRV5056-Q1 Hi team,
My customer wants to minimize voltage noise. Are there any other effective measures besides the bypass capacitor and RC filter in the block diagram?
Regards,
Part Number: DRV5056-Q1 Other Parts Discussed in Thread: TMAG5170 , DRV5056 , DRV5055
Hi,
I am looking for optimal option for magnet dimensions and material( N35/N38 ) for below criteria.
I have concern as the distance increases, the resolution…