Part Number: DRV5057 Tool/software: I got this part DRV5057A4 QDBZR from mouser electronics . The part is in SOT 23 package and 57A4 is etched on the chip. When i connected the the to 5V DC and checked the ouptut pin by connecting an oscillosope we cant…
Part Number: DRV5057-Q1 Other Parts Discussed in Thread: DRV5057 , DRV5055-Q1 , DRV5056-Q1 Hi, we would like to use a hall sensor to measure the distance between two parts.
Current our space design is shown below.
The design gap between hall sensor…
Part Number: DRV5057
Tool/software:
Hi, We are looking for linear hall sensors with digital outputs. The DRV5057 family seems to be a good candidate for us. But it seems all of the SOT variants are no more in production and only custom reels are available…
Part Number: DRV5057 Hi Texas Instruments Technical support where can I find a Cylinder magnet: 4.7625mm diameter, 12.7mm thick, neodymium N52, Br = 1480 for DRV5057
Regards
Yesaiahu redler
Part Number: DRV5057-Q1 Tool/software: Hi, I am trying to get measurements from a DRV5057-A4EDBZRQ1 sensor. It should output a PWM signal but instead, I am getting a constant signal of 5V.
I made the circuit as described in the datasheet. One decoupling…
Part Number: DRV5057 Hello,
I used DRV5057 for the sensing position. It works fine,
But it gives a 50% duty cycle of its output when there is no magnet present.
My requirement is, I want to output with duty cycle 0 to 100% which linearly vary with…
Ella,
Using the PWM output of the DRV5057 as a motor driver is not a use we have seen. The maximum continuous output current is only 20 mA, and my understanding is that motors require a somewhat more complicated PWM input for proper motor control. …
Part Number: DRV5057 Hi, For my project I would Ideally like to use the DRV5057A1QDBZ, unfortunately this part is out of stock at every shop I can find. From searching around I have seen that in stock are DRV5057Z1QDBZ (without temperature compensation…
Part Number: DRV5057 Other Parts Discussed in Thread: , DRV5055-Q1 Hi team,
The customer uses DRV5057 as the sensor chip of the brake foot valve. Foot valve is required to output 2 complementary PWM signals. Customer would like to know If he uses two…
Part Number: DRV5057-Q1 Other Parts Discussed in Thread: DRV5057 Hello, I am developing a brake system. I am going to make a product that outputs a brake signal using a magnet and a hall sensor.
I am going to make a brake product that is resistant to…