Part Number: DRV5057 Other Parts Discussed in Thread: , DRV5055-Q1 Hi team,
The customer uses DRV5057 as the sensor chip of the brake foot valve. Foot valve is required to output 2 complementary PWM signals. Customer would like to know If he uses two DRV5057…
Part Number: DRV5057 Hi team,
I wonder if DRV5057 has use cases that are used for motor driving application. I don't think there will be no functional concern in hall-effect sensor, but i wonder if it's usual to use this part for motor driving, because…
Part Number: DRV5057 Other Parts Discussed in Thread: DRV5055 , Figure 18 on the data sheet shows which side of the IC is approached by the S-pole when looking at the IC from the top surface?
I have the same diagram in the DRV5055 data sheet, can you tell…
Part Number: DRV5057-Q1 Please provide links to vendors of small magnets that are typically used with TI Hall Effect sensors. I am looking for magnets that are < 2mm in diameter and < 2mm long. Thank you!
Part Number: DRV5057 Hi team,
My customer considers to use DRV5057 and he is asking a question.
The datasheet states that Sensitivity linearity error "SLE" is ±1%(typ).
The ±1% here is a percentage of what value?
Best regards…
Part Number: DRV5057 Hi Team, Need your expertise on our customer's query. They would like to work with our linear hall effect sensors but would like to initially know the possible effects or implications on the performance of the device upon being exposed…
Part Number: DRV5057 The data sheet shows a linear magnetic detection range for Vcc = 5 V, but what is the value for Vcc = 3.3 V?
I am assuming the following values.
Are they correct?
DRV5057A1 : ±35mT
DRV5057A2 : ±70mT
DRV5057A3 : ±14…
Part Number: DRV5057 Other Parts Discussed in Thread: DRV5055-ANGLE-EVM Hi teams
My customer used a switch hall sensor in BLDC to achieve speed/location detection. But in order to further enhance the resolution and accuracy of the measurement, they plan…
Part Number: DRV5055 Other Parts Discussed in Thread: DRV5057 Tool/software: Hi,
When I try to do a simulation in the webench.ti.com/.../ environment, there is no output. When I change the sensor to a drv5057 I do get outputs for every sensor, but adding…