Other Parts Discussed in Thread: DRV595 , DRV595EVM I have a simple application simulating an AC generator. The requirement is to drive a 4 ohm load with about 0.6A RMS (2.4W) max (zero up to that level) at frequencies between 55 and 65 Hz. I selected a…
Other Parts Discussed in Thread: DRV595EVM , DRV595 Hello,
Please answer following questions.
< Q1 >
Datasheet title is “15V/±4A High-Efficiency PWM Power Driver”.
What is the meaning of “15V” ?
< Q2 >
Question…