Part Number: DRV603
Hi Team,
customer would like to design DRV603 in TV to driver line out or headphone out.
Would you please review schematic/questions and provide your comment?
(1)can DRV603 support headphone output 5mW with Load 32Ω?
(2) can…
Part Number: DRV603 Other Parts Discussed in Thread: TPA6130A2 , TPA6138A2 , Hi,
We are evaluating amplifiers for a high impedance headphone (200 Ohm) application. We are mainly concerned with output power at this time, before evaluating noise and quality…
Part Number: DRV603 Other Parts Discussed in Thread: TPA6133A2 , TPA6112A2 Hi Sir,
Could you please advise us a candidate which can compare with MAXIM MAX97220?
Here are the requirements from our customer, they would like to find a part which can drive…
Part Number: DRV602 Other Parts Discussed in Thread: DRV603 Dear Sirs,
My Customer asked us about "Noise Floor" of DRV602 and DRV603.
There is an item of "Noise Figure" in the comparative chart of ti website below, but it is not in the data…
Part Number: DRV603 I like the concept of the integrated charge pump which theoretically allows negative output voltages with unipolar supply. That’s why I’d like to use the DRV603 as a pitch CV output driver for an electronic music instrument. The input…
Part Number: DRV603 Hi all Would you mind if we ask DRV603PW? The customer consider using this device with Figure 13 configuration.(as second differential amplifier) DRV inputs connect to DAC output. DAC's offset is 2.5V. <Question> The customer would…
SCHEMATIC1 _ 09_DSP 0 MCASP.pdf Hi Ivan sir
I have further question for this issue. Here is the story for this issue until now.
Issue Description:
One NG board, returned from our customer, has no audio function and we confirmed that audio amplifier U4…
Part Number: DRV603
Hi team,
I have a few questions regarding DRV603 output loading. The datasheet states maximum output current is 20mA (typ) - is this peak current? Or continuous DC?
What is the minimum resistance value required on the output of DRV603…
Hi Cherry,
Another applications engineer has had this same request before. the charge pump frequency cannot be modified,
However the device DRV603 is pin-for-pin compatible and has a higher typical charge pump frequency
Regards, Arthur