Part Number: DRV632 Hi LPAA team
What is DRV642 background? Could it be used to directly drop in to replace existing customer DRV632 design?
Thanks!
-Rocky
Part Number: DRV632 Hi Team,
The customer is experiencing below issue and needs your help.
1: The pin has MUTE pin, and the application circuit is EN pin, without MUTE pin, are these two equivalent?
2:Whether the accessory circuit is correct and whether…
Part Number: DRV632 Hi team,
In current, I had a question with DRV632.
our schematic is below.
for audio frequency response of RMS value test
My test result(use 1k sine wave as 0dB reference)
20Hz->-2dB
1kHz->0dB
20kHz->-0.09dB
I need to adjust…
Part Number: DRV632 Other Parts Discussed in Thread: TPA6138A2 Dear team,
Customer wonder what application may use DRV632?
They found the internal structure of DRV632 and TPA6138A2 is similar. During their application, they must have a headset PA, so…
Part Number: DRV632 Hi team,
I wondering what is the purpose for R3 and C1 at the reference circuit for second order low pass filter, can we remove it?
Part Number: DRV632 Hi team,
When I used DRV632 to P2P replace AD22650 from AD22650 in the wireless microphone receiver in the same board, it was found that The audio signal of wireless microphone receiver will be disconnected occasionally When I put…
Other Parts Discussed in Thread: TAS5558 , DRV632 , TAS5342 , TAS5634 , TAS5548 , TPA6138A2 Hi everyone,
our circuit design is by TAS5558 and DRV632, when the tas5558 chip code initial , the active subwoofer will produce the patter nosie。
could you give me…
Part Number: DRV632 Other Parts Discussed in Thread: DRV603 Hi,
DRV632 is a line driver according to datasheet, what is line driver? because it has a charge pump inside? And what is the difference between OPA and line driver?
Thanks.
Best regards
…