Part Number: DRV81008-Q1 13.5V KL30 power is applied on IN1 pin of DRV81008 through 10Kohm resistor. Will IN1 pin be damaged by this high voltage for 2 cases? Case1: when VDD power is not available and VS pin is powered by 13.5V KL30 power. Case2: when…
Part Number: DRV81008-Q1 Hello team,
Are we able to use DRV81008-Q1 for the below use case? I read the datasheet, but I am not sure if DRV81008-Q1 can be applied and how to achieve it.
Best regards,
Shotaro Sakai
Part Number: DRV81008-Q1
Tool/software:
Dear Sir/Madam,
Is there any issue with VCC=3.3, VM=5V and INx connected to 12V inductive load? Will the gate drive still allow 330mA and be over voltage protected VM_AZ 42V to 53V? Also does all the reporting…
Part Number: DRV81008-Q1 Tool/software: Hi team,
Could you please provide the typ value of the thermal pad dimension circled in red? It only specified max value in datasheet, but my customer need typ value for internal device qualification.
Thank…
Part Number: DRV81008-Q1 Tool/software: Hello team,
It is described in the ds that DRV81008 supporting SPI daisy chain, do we need configure any registers to enable or control the function?
Regards,
Daniel Wang
Part Number: DRV8803 Other Parts Discussed in Thread: DRV81008-Q1 , DRV81004-Q1 , DRV8243-Q1 Tool/software: Hi Expert,
Do we have auto version of DRV8803? Please recommend the most similar auto device to replace DRV8803 if DRV8803 haven't auto version…