Part Number: DRV8106-Q1 Other Parts Discussed in Thread: DRV8243-Q1 , Hi,
DRV8243-Q1 datasheet (Section 6.7.2 of Rev.C) shows timing constraints for the CLR_FLT command. I would like to confirm if this is applicable to DRV8106-Q1 also. I couldn’t find…
Part Number: DRV8106-Q1 Other Parts Discussed in Thread: TPS7B81-Q1 Tool/software: Hello Team,
We are planning to use the DRV8106-Q1 in our design to drive an inductive load. According to the datasheet, it has an input offset voltage of +/- 3.5 mV at…
Part Number: DRV8106-Q1 Other Parts Discussed in Thread: DRV8706-Q1 Tool/software: I would like to estimate the delay time that I_GLx(I_GL_x=I_HOLD) reflects V_INx change(Hi->Lo) on "Figure 7-5. TDRIVE State Machine".
(I would like to ask the same for…
Part Number: DRV8106-Q1 Tool/software: Hi,
I have configured the UVOV_CTRL register with the value 0xF4 . With this setting, I observed that the FAULT pin is asserted when the power supply voltage exceeds 28.5 V . However, the corresponding fault bit…
Part Number: DRV8106-Q1 Tool/software: It is said that high side and low side are dependent in hardware version. I would like to use the hardware controlled version of DRV8106 as a independent high side driver for 100% PWM without switching on low side…
Part Number: DRV8106-Q1 Other Parts Discussed in Thread: DRV8706-Q1 Tool/software: I have the following queries regarding DRV8106S and would request your urgent attention for the same.
We are planning to use DRV8106S with independent High side and low…
Part Number: DRV8106-Q1 Ive the same behavior for all register, first read aftec POR send back default value written into datasheet, second read give 0x00.
This is true when ever I read all register once, then redo reading loop, or reading a single…
Part Number: DRV8106-Q1 I'm evalutation DRV8106 Q1,
I manage to configure and start the HBridge, I've a 50% PWM @ 2 KHz on IN1.
I've command signal on GH1, and high side MOS is driven accordingly
No fault repoorted
CSA configured and current reading…
Part Number: DRV8106-Q1 Other Parts Discussed in Thread: DRV8706S-Q1EVM , UCC25600 Hi, I'm currently doing an automotive new design and I have some concerns regarding the DRV8106-Q1. I was wondering if someone faced the same issues and could help me with…