Part Number: DRV81080-Q1
Dear TI Team,
Does TI have AEC-Q100-012 characterization data or equivalent short-circuit reliability data for DRV81080-Q1 ?
If available, could you please provide:
Maximum short-circuit activation count corresponding…
Part Number: DRV81080-Q1 Hello TI Team,
I would like to know the parasitic capacitance characteristics of the internal MOSFET in DRV81080-Q1.
For discrete MOSFETs, datasheets often provide Ciss, Coss, and Crss versus VDS curves.
Could you…
Part Number: DRV81080-Q1 Hi TI Support Team,
I have a few questions regarding the Open Load at ON (OLON) diagnostic feature on the DRV81080-Q1:
Channel Availability in EN_OLON Register: The Open Load at ON Register (Table 7-26) provides 8 status…
Part Number: DRV81080-Q1
Hi TI Team,
I would like to confirm the behavior of the SDO pin when the DRV81080-Q1 is in Sleep mode.
According to the datasheet, SPI communication is disabled in Sleep mode, and there are descriptions indicating that the…
Part Number: DRV81080-Q1
Hello TI Team,
I would like to understand the internal operation of DRV81080-Q1 when a channel is inactive (OFF state).
- Is the internal MOSFET completely turned off during the inactive state?
- Is the charge pump…
Part Number: DRV81080-Q1
Hello TI Team,
We are evaluating the DRV81080-Q1 for driving an automotive relay.
We would like to understand the back EMF protection capability of the device. When the relay coil is turned off, a reverse voltage (inductive…
Part Number: DRV81080-Q1 Hi TI team,
According to the application example in the datasheet, the 10 nF capacitor on each output pin is intended to protect the device against ESD and BCI events.
Could you please clarify whether the device is expected…
Other Parts Discussed in Thread: DRV81080-Q1 , DRV81080-Q1EVM
Hi TI Team,
I have a question regarding unused pins on the DRV81080-Q1.
NC pins
Could you please clarify the recommended handling of the NC (No Connect) pins?
Should all NC pins…
Part Number: DRV81080-Q1 Dear TI Team,
We would like to confirm the robustness of the DRV81080-Q1 under ISO 7637-2 Pulse 1 negative surge conditions.
We are considering the following power supply configuration:
VM is connected to the Battery line…
Part Number: DRV81080-Q1 Hi TI team, In the schematic, the controller is connected to the DRV81080-Q1 through series resistors only. Is any external pull-up supply circuit required for the interface signals (nSLEEP, IN0, IN1, nSCS, SCLK, SDI, and SDO…