Part Number: DRV8145-Q1 Tool/software: nFAULT pin is low continuously, until the nSLEEP is low. When nSLEEP return to high the fault is low.
SR = 0E
DIAG = 0E
IPROPI = 4.1K
ITRIP = 100K
VCP = 29V
DRVOFF = 0V
With out load(motor rated at 250mA) output…
Part Number: DRV8145-Q1 Other Parts Discussed in Thread: DRV8243-Q1 , Tool/software: Hello team,
Regarding negative voltage abs max of VM of DRV8145-Q1 and drv8243-Q1, there is a note below.
"With external component support, short duration violation of…
Part Number: DRV8145-Q1 Tool/software: Hi!
I wish to use two DRV8145 as an H-bridge, driving a single phase BLDC at 36V 35A up to 150K RPM. I intend to set them up as per the datasheet (image below).
I intend to feed both half bridges with the same 125…
Part Number: DRV8145-Q1 Tool/software: Hello team,
Is thermal Pad of DRV8145P-Q1(HTSSOP Package) GND? (or at least, Can thermal pad be connected to GND?)
Regards,
Hirata
Part Number: DRV8145-Q1 TI Team,
in below desciption of OLP, what is the meaning of "output short" and "load short".
How this conditions are defined, and what are diferences between them?
Part Number: DRV8145-Q1 Hi Team,
How to terminate DRVOFF pin when DRVOFF pin is not needed?
Datahseet describes tied off low.
However, DRVOFF pin has internal pull-up.
if we connect DRVOFF to low(tied to GND), there may be unnessesary leak current so…
Part Number: DRV8145-Q1 Hey Team,
I'm trying to apply 4 DRV8145 in parallel operation but the current trip function does not function properly because one of the IC's keeps going into OCP mode and closes entirely at current trip, so the other one keeps…
Part Number: DRV8145-Q1 Hi,
I am doing a new layout and adding the following as part of my design. However I cannot find the .stp file anywhere for VQFN-HR (RXZ) | 16 Can you please link the .stp file. Thanks,
Tom
Part Number: DRV8145-Q1 Other Parts Discussed in Thread: DRV8144-Q1 Hello,
Can I use the DRV8145 for the purpose of driving this foil rated at 12V 100W ?
The driving frequency should be around just 200Hz.
Thanks in advance.
Best,