Part Number: DRV8210 Other Parts Discussed in Thread: TPS631000 Hi
In the following graph, the blue signal is the IN1 and the yellow signal is OUT1.
When the solenoid is not connected, the signals are smooth and clean. However, when the solenoid is connected…
Part Number: DRV8210 This is Youssef Elbadri from the research and development department (I-D Tech) of Nile University, one of the leading universities in engineering in Egypt and the MENA region (See our website: www.nu.edu.eg/home-page).
We are currently…
Hello,
If it is voltage/current spikes, it could be possible that OCP (over current protection) is triggering if the current is above the OCP threshold. One way to check if this is the root cause it to add some resistance in series with your load and…
Hello Gabriel,
Any updates? I'm going to close this thread due to inactivity. Please reply back or post a new related question for further support.
Regards,
Pablo Armet
Part Number: DRV8210 Other Parts Discussed in Thread: DRV8220 Hello,
I urgently require x20 DRV8210DSGR IC's - is it possible to obtain these?
Need to possess ability to provide at least +11V/12V output
Part Number: DRV8210 Hi experts,
Customer will use 1.8V pulse for control input. I think it is ok since above 1.45V with the situation 1.65V<VM<11V in 7.5 Electrical Characteristics.
I would like to make sure 1.8V logic high is ok for 3.3V VM, correct…
Part Number: DRV8210 Other Parts Discussed in Thread: DRV8838 , Hi! I have a weird problem with DRV mode selection: When device is powered up it can operate only in half-bridge and PWM modes and I can't turn on PH/EN mode in any way other than holding mode…
Part Number: DRV8210 Other Parts Discussed in Thread: , DRV8220 I have question about DRV8210, DRV8210P, and DRV8220.
These IC's dead time (tDEAD) are larger than propagation delay (tPD), but I have seen the other motor driver are almost tPD > tDEAD.…