Hi Orlando,
Thanks for posting in this forum.
Orlando Diaz said: Is the exposed thermal pad electrically connected to GND internally, or is it thermal‑only?
Not electrically connected to GND internally. It is thermal only metal tab that mechanically…
Part Number: DRV8242-Q1 Tool/software: For DRV8242-Q1, Maximum load current mentioned in the datasheet is 6A (max) but the current gain is specified up to an output current (Io) of 2A. Can this part be used for a load current of 3A?
Part Number: DRV8242-Q1 Hi team,
My customer is looking for DRV8242 Pin1 ID dimension for new device qualification. Could you provide dimension of each legs of Pin1 ID?
Thank you,
Muwei Zheng
Part Number: DRV8242-Q1 Other Parts Discussed in Thread: DRV8873 , DRV8243-Q1 , Hi team,
May I know if we have any device can meet nelow requirements?
Supply voltage: 12V
Logic voltage: 3.3V
Current: >2A
The competitor is attached.
RZ7899…
Part Number: DRV8242-Q1 Tool/software: Hello,
Could you tell me what is the longevity or how many years from now Texas Instruments will continue to make the following components?
1. DRV8242HQRHLRQ1;
2. DRV8242PQRHLRQ1;
3. DRV8242SQRHLRQ1;
4…
Part Number: DRV8242-Q1 Hi team,
My customer is using DRV8242S-Q1, they want to disable the ITRIP function for first 10ms, and then program it to another value. The goal is to avoid start up failure due to current limit.
According to datasheet, S_ITRIP…
Part Number: DRV8242-Q1 Tool/software: Hi team,
Do we have any special requirements for the time interval from t5 nFAULT pull-up to nSLEEP pull-up?
My customer found in the test that when this interval is 10us, the nFAULT will be pulled down again…
Part Number: DRV8242-Q1 Tool/software: Hi team,
Could you please help check below questions about DRV8242-Q1? Thanks in advance.
1. If the DRVOFF pin can be pulled down directly to the ground? And only works in the following mode marked in green…
Part Number: DRV8242-Q1 Other Parts Discussed in Thread: DRV8243-Q1 , Hi team,
Customer wants to degrade DRV8243-Q1 to DRV8242-Q1 in their system. May I know besides the MOSFET RDSON, is there any other spec difference? and do they need to do any software…