Part Number: DRV8243H-Q1EVM Tool/software: When considering RPROPI values from DRV8243-Q1EVM, the ITRIP values will be in microamperes (µA). For a motor load current requirement of 3A, calculation using the maximum VTRIP value resulted in a very low RPROPI…
Part Number: DRV8243H-Q1EVM Other Parts Discussed in Thread: PCF8574 , ADS1115 , DRV8243-Q1 Tool/software: Hello Joshua, months ago I opened a thread "DRV8243H-Q1EVM: general configuration & layout revision".
I build some pcb boards according to schema…
Part Number: DRV8243H-Q1EVM Other Parts Discussed in Thread: DRV8243-Q1 Tool/software: Hi!
I want to combine the sleep/drvoff inputs and the fault outputs of two DRV824xH-motor drivers: one DRV8243H and one DRV8244H (see schematic, caps and pullups…
Hi JM,
Would you mind providing a block diagram of your application? I would like to check your load configuration. The DRV8243 cannot support parallel output on the same device. To achieve this the DRV8143 would need to be used.
Juan Journade said…
Part Number: DRV8243H-Q1EVM Tool/software: We're using the DRV8243HQRXYRQ1 in a full-bridge configuration to drive an actuator. We've set the overcurrent protection to its maximum limit, but the device is tripping at 6.5A, significantly lower than our…
Part Number: DRV8243H-Q1EVM Other Parts Discussed in Thread: MSP430G2553 Tool/software: I am using DRV8243H-Q1 EVM. I am selecting 20KHz frequency but I am getting only 2.5KHz PWM output. I am getting proper frequency output at 10KHz, 5KHz and 2.5KHz…
Part Number: DRV8243H-Q1EVM I recently acquired the DRV8243H along with the EVM, and I'm encountering two issues:
Currently, the nFault is triggered when the ITRIP reaches 5A, and I'm struggling to adjust it to a different value. I've attempted…
Part Number: DRV8243H-Q1EVM Other Parts Discussed in Thread: DRV3946-Q1 Tool/software: I have started to evaluate the DRV8243 H variant for a project. I downloaded the simulation for it an run it, but when I look at the IPROPI voltage, it seems to go…
Part Number: DRV8243H-Q1EVM Is the rising edge of nFAULT only a sure indication for a ClearFault or also for a wake up during the NSLEEP pulse? The reason for the question is to minimize the time for the NSLEEP pulse, which is stated as 20µs to 40µs.…
Part Number: DRV8243H-Q1EVM Other Parts Discussed in Thread: LM74610-Q1 Hello everyone,
I have a DRV8243H-Q1EVM. When I connect a motor and operate the bridge with PWM, I have periodic voltage drops on the output side.
The signals can be seen on the…