Part Number: DRV8243S-Q1LEVM Other Parts Discussed in Thread: INA229 Hi,
I'm evaluating the DRV8243S circuit with the evaluation kit DRV8243S-Q1LEVM. I will attach the current test setup and oscilloscope pictures below.
For some reason there is a…
Part Number: DRV8243S-Q1LEVM Other Parts Discussed in Thread: DRV8243-Q1 Hello,
For DRV8243SQRXYRQ1, is there any necessity to add High Value Series Resistor on Control Input Pins, and also on SPI Pins? If yes, what is the reason? For SPI usually a…
Hi Anjali,
Anjali Karmude said: PFB the schematic screenshots.
The schematic looks good, I do not see anything that could be causing this issue.
Regards,
Joshua
Part Number: DRV8243S-Q1LEVM
Hi Team,
Posting on behalf of our customer.
As per device data sheet, SLEEP pin voltage is also VIO logic level for SDO. But we measured the SDO voltage is much lower than V_nSLEEP. Could you please support to check…
Part Number: DRV8243S-Q1LEVM Other Parts Discussed in Thread: MSPM0L1306 , , DRV8243-Q1 , MSPM0G3507 Hi all, I would like to program the MSPM0L1306 to communicate with the motor driver DRV8243S via SPI, so it drives the motor for 50ms. My question is…
Part Number: DRV8243S-Q1LEVM Hi,
Our customer encountered some issues while debugging the BDC driver chip DRV8243S, as follows:
When attempting to switch the driver chip from sleep mode to standby mode, raise the nSleep pin and send CLR _ FLT cmd…
Part Number: DRV8243S-Q1LEVM Hi team, customer use DRV8243S-Q1LEVM to do OCP test. but they find that OLA is asserted mistakenly when OCP removed, which is presented only in PH/EN mode and is normal in PWM mode. could you help me to find the reason of…
Part Number: DRV8243S-Q1LEVM Hello team,
My customer is using DRV8243 to drive solenoid. (They are driving the solenoid with H bridge)
However, they are experiencing increase in VM (up to 35V) when fast decay mode.
Is there any ways to reduce…
Part Number: DRV8243S-Q1LEVM Other Parts Discussed in Thread: DRV8243-Q1 Hi team,
My customer replied that they used the DRV8243-Q1 EVM function to tell short circuit issue or open circuit issue but the device didn't support the function. So I want…
Part Number: DRV8243S-Q1LEVM Hi Team,
A customer was unable to connect the EVM to their PC because of the issue below, can you help troubleshoot?
They connect the tool to a computer via USB and start GUI Application. Then choose icon "DRV824xS/P…