Part Number: DRV8245-Q1 Other Parts Discussed in Thread: DRV8144-Q1 , DRV8145-Q1 Tool/software: Hi Expert,
Have a nice day!
DRV8245-Q1’s Iout(max) is 32A, does it mean it can support 32A continues current for long time?
Thanks!
Best Wishes…
Part Number: DRV8245-Q1 Tool/software: Hello,
I have a doubt on controlling of H bridge.
In mode table there are three modes, I want to understand that
In what application i should use PH/EN and PWM mode?
What is the difference between PH/EN…
Part Number: DRV8245-Q1 Tool/software: Hello.
Iam trying to see how DRV8245 behave on short to GND condition, DRV8245 is configured as independent mode.
The max. OCP according to datasheet is 64A but, the peak current is going up to 65A. Why?
…
Hi Nicolas
Can you check the voltage at the DIAG pin as close to the pin as possible? I understand that the pin is pulled to GND but would like to be sure this is the case.
If you have a device on a different PCB, like our DRV8245H-Q1EVM, which…
Part Number: DRV8245-Q1 Tool/software: Dears,
The customer uses DRV8245 in the project. Usage mode: 1, PH/EN mode, one full-bridge output 2, independent mode, independent control of two half-bridges, output of two PWM channels respectively
Functions…
Hi Luca,
Thank you for your post.
Luca Meloni said: This motor operates at 13.7 volts, with a nominal current of 10 amps. I wanted to know if the chosen driver is suitable for this motor.
I assume this means continuous current requirement for this…
Part Number: DRV8245-Q1 Other Parts Discussed in Thread: DRV8245S-Q1LEVM , Tool/software: I would like to ask if there is any sample code or reference material for DRV8245s-Q1 Driver IC.
Datasheet is being obtained and reviewed, but it is difficult…
Part Number: DRV8245-Q1 Other Parts Discussed in Thread: DRV8244-Q1 , DRV8243-Q1 , Tool/software: Hello experts,
Our customer is using DRV8245PQPWPRQ1 now, but would like to know whether all fault protection and diagnosis functions are same among DRV8243…
Part Number: DRV8245-Q1 Tool/software: Hello,
Is the total standby current of the driver (Istandby) mentioned in section 8.4.2 of the datasheet the same as IVMS (table 7.5.1)?
Thanks
Part Number: DRV8245-Q1 Tool/software: Hello,
Just want to verify that OLP reference high and low values shown in table 7.5.12 of datasheet are set values and not dependent on any inputs?
Thanks