Part Number: DRV8245-Q1 Tool/software: Hello,
Just want to verify that OLP reference high and low values shown in table 7.5.12 of datasheet are set values and not dependent on any inputs?
Thanks
Part Number: DRV8245-Q1 Tool/software: Hello,
Can you please share EMC reports for the DRV8245 motor drivers' family (specifically the HW variants)
Currently we are seeing some issues at the BCI test and wanted to see how the Ipropi pin performs under…
Part Number: DRV8245-Q1 Hello. I would like to ask about DRV8245-Q1 device. 1. In SPI(P), (VM undervoltage translators) is a question about how long and how much voltage it is. 2. Apart from the SPI connection, which pins should be essential to the MCU…
Part Number: DRV8245-Q1 Tool/software: Hi team,
DRV824X hardware version could be used for both clear fault and mode transition to sleep. May I know if there's not fault, when sending 5~20us reset pulse, it will not influence normal operation right…
Part Number: DRV8245-Q1
for drv8245-q1 rxz0016a package, we provide 1 max thickness like the picture, could you provide min value for customer process engineering request?
best regards,
jeff wang
Part Number: DRV8245-Q1 Tool/software: Hi team,
I have a question about the max current ratings of body diode of the main FET.
Is there max current ratings for the body diode, or is it fine as far as the junction temperature is <150c?
In my case…
Part Number: DRV8245-Q1 Tool/software: Hi, I have a project with a DC-motor consuming around 3A when running on maximum load which apparently is far beyond what we can get with the evaluation kit of DRV8245-Q1. This DC-motor driver was supposed to be…
Part Number: DRV8245-Q1 Other Parts Discussed in Thread: DRV8145-Q1 Tool/software: The motor parameter as below table, please help check can DRV8245-Q1 meet the motor requirement?
Part Number: DRV8245-Q1 Tool/software: I saw part-number with SN824x, is SN824x the same DRV824x? Thanks?
SN8245HQRXZRQ1 =DRV 8245HQRXZRQ1 ?
SN8244HQRYJRQ1 =DRV 8244HQRYJRQ1 ?
SN8243HQRXYRQ1 =DRV 8243HQRXYRQ1 ?
Part Number: DRV8245-Q1 Other Parts Discussed in Thread: MSP430G2553 Tool/software: Hello all,
I plan to use the DRV8245-Q1 in SPI(S) mode and PH/EN mode. I wanted to test it with a most simple configuration. I build a PoC on breadboard, but with no…