Part Number: DRV8245H-Q1EVM Tool/software: hi,
Can I perform short to battery diagnosis when using DRV8245H version;According to my idea, the SENSE on the high side cannot sense the overcurrent of the low side measurement。
Part Number: DRV8245H-Q1EVM Hi
We found there is a Script window at the DRV824x GUI.
But can't found any resource to help us to control DRV8245 by the Script Window.
Any resouce could suggest?
Part Number: DRV8245H-Q1EVM Other Parts Discussed in Thread: DRV8434 Hello Team:
DRV8245H-Q1EVM
DIAG pin set to LVL1 (Fault reaction in Retry mode), Motor stall, nFAULT LED on, OUT1/OUT2 no power off, The motor is in a stalled state.
DIAG pin set to LVL2…
Part Number: DRV8245H-Q1EVM Hi Team,
1) According to the documentation, neither PWM mode nor stand-alone mode is supported. However, it is on at LVL1 of demo board mode1 and the LVL2LVL3 has no effect with the jumper attached. The customer would like to…
Part Number: DRV8245H-Q1EVM Hi team,
I am connecting the DRV8245H-Q1EVM with an external MCU. So I have removed all the 0 ohm resistor in area 1. I am trying the independent mode, so I gave nSLEEP, IN1 3.3V voltage and IN2, DRVOFF 0V as the datasheet…
Part Number: DRV8245H-Q1EVM Other Parts Discussed in Thread: DRV8245-Q1 Hi Team
I am trying to apply the electromagnetic brake with the DRV8245-Q1.
I want to control the current by feeding back the current flowing through the electromagnetic brake, but…
Part Number: DRV8245H-Q1EVM Other Parts Discussed in Thread: DRV8245-Q1 Hi team,
DRV8245-Q1 datasheet(HW Variant in VQFN-HR Package) page62(pin7-out1, pin6-GND) and page8(pin7-GND, pin6-OUT2) are paradox
Could you help clarify which pin numbers are correct…
Part Number: DRV8245-Q1 Other Parts Discussed in Thread: DRV8245H-Q1EVM Tool/software: Hi, We are seeing an issue in our design where we are unable to drive any outputs of the DRV8245 (hardware variant). The startup sequence is: 1. Put device into sleep…
Hi Wipop,
The math looks right. We do have EVM's available for the DRV8245, which can be used for bringing up of your board:
DRV8245H-Q1EVM Evaluation board | TI.com
Best,
Keerthi
Hey Prema,
prema R said: What is the maximum current the chip DRV8873-Q1 can sustain?
For continuous operation, this will depend on the thermal limitation of the device which is affected by the PCB layout and if you're using external heatsinks. See the…