Part Number: DRV8256EEVM Other Parts Discussed in Thread: DRV8256 , DRV8256PEVM We are developing a product which is driving the Brushed DC motor. For that we have used the reference of the DRV8256EEVM Evaluation board.
Motor Specification:
…
Part Number: DRV8256EEVM Hi team,
Here's some issues may need your help:
1) Regarding the drive waveform of 8256E, the description in spec is "The EN input drives the waveform PWM, and the PH pin inputs the direction signal so that out1 and out2 output…
Part Number: DRV8256EEVM Other Parts Discussed in Thread: DRV8436 ****** SO# 704529 *****
Hello,
one of our customers purchased this board and states that a wrong chip is mounted on the board, as it includes a DRV8436 instead of a DRV8256E....
Please…
Other Parts Discussed in Thread: DRV8256EEVM , DRV8711 Hi TI,
I am working on Machine control project in that project we are going to use stepper motor and universal motor ..... I am requesting you to suggest me the correct driver part no and
evaluation…
Part Number: DRV8256PEVM Other Parts Discussed in Thread: DRV8256EEVM Hi
I want to purchase DRV8256PEVM, and I checked the BOM of this.
DRV8256EPWPR was described in the BOM of DRV8256PEVM. I think DRV8256PPWPR should be used in DRV8256PEVM.
I think…
Part Number: DRV8256 Other Parts Discussed in Thread: , DRV8424 Hello, The datasheet mentions that 3.3V logic levels are supported but I don't see any mention of how to support those logic levels. The datasheet says the Vih ranges from 1.5V to 5.5V so…
Hi Rock,
Based on the current needs of 3A continuous, the DRV8256 looks like a good replacement for the L6208. The DRV8256 can handle up to 5A continuous. The DRV8256 has an operating voltage of 4.5V - 48V which is slightly lower than the L6208. If…