Part Number: DRV8256 Dear Sirs,
We assembled some prototypes for using the DRV8256PWPR to drive motors.
It turns out that now, we are having difficulty activating the outputs of the integrated circuit.
Even switching the IN1 and IN2 pins to 1 and 0,…
Part Number: DRV8256EEVM Other Parts Discussed in Thread: DRV8256 , DRV8256PEVM We are developing a product which is driving the Brushed DC motor. For that we have used the reference of the DRV8256EEVM Evaluation board.
Motor Specification:
Motor Voltage…
Hi Rock,
Based on the current needs of 3A continuous, the DRV8256 looks like a good replacement for the L6208. The DRV8256 can handle up to 5A continuous. The DRV8256 has an operating voltage of 4.5V - 48V which is slightly lower than the L6208. If you…