Part Number: DRV8263S-Q1EVM Hi,
I'm using DRV824x_DRV814x_DRV8x63-Q1EVM-GUI v1.10.1 to test the DRV8263S-Q1EVM.
It let me drive the DRV8263 but I'm facing limitations to tune PWM frequencies and slew rates.
For both, only "droplist" allows to…
Part Number: DRV8263S-Q1EVM Other Parts Discussed in Thread: MSPM0G3519 , SYSCONFIG Hi,
Hi Joshua,
I replaced the GUI with MSPM0G3519 SPI Master. As you suggested above, the CLR Fault command generated from the SPI master (without connecting the DRV8263S…
Hi Sakhan,
Sakhan said: Is the correct approach to have MSPM0 replicate the same SPI register write sequence performed by the GUI during initialization and runtime?
This is a good approach although there is no specific write sequence that needs to…
Part Number: DRV8263S-Q1EVM Tool/software: Hello,
Is DRV8263S-Q1EVM available for 48V operation?
Seeing from EVM users guide, we cannot support 48V.
In the website it is said the max. operational voltage is 65V.
Part Number: DRV8263S-Q1EVM Other Parts Discussed in Thread: DRV8263-Q1 Tool/software: Hi,
we want to use the new DRV8263S-Q1 (SPI version) in our new project and already tested the dev board. When will there be parts (or at least samples) be available…
Part Number: DRV8263S-Q1EVM Other Parts Discussed in Thread: DRV8263-Q1 Tool/software: Hi,
I am using this part in our design and would like to obtain some information regarding the failure mode distribution % that is needed for a FMEA and the FIT rates…
Part Number: DRV8263S-Q1EVM Other Parts Discussed in Thread: DRV8263-Q1 , Tool/software: Hello team,
I'd like to control a 12V BDC motor using DRV8263S-Q1 through SPI with MSPM0. However, I'm not sure if this driver can be connected to MCU. Is it…
Hi Michael,
This is a known mistake in the user's guide for this device that will be fixed. The DRV8163-Q1EVM and DRV8263-Q1EVMs are designed to be able to accept input up to 70V max.
You can supply 48V to the DRV8163-Q1EVM board and the board will…
Hi Mojtaba Afshar ,
The DRV89xx-Q1 with builtin PWM generator looks very nice and promising for the 24V actuators.Thank you.
It appears that a EVM for the DRV8263 SPI interface variant is unavailable or has special status as limited qty. https:…
Hi Jishnu,
Jishnu K. said: My application is in 60 degree Celsius, Is it possible to use for this application?
Is there any SOA that defined at different voltages for DRV8263?
This is defined by the power dissipation of the application which is…