Part Number: DRV8301-69M-KIT Hi, We are developing a powertrain / drivetrain in piccolo F28069M using SpinTAC libraries and we have two drive modes like ECO and SPORT. Is there any internal variable to improve the torque apart from the User_IqRef which…
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: DRV8301 Hello,
In our design, when the system (Application) is in idle state we put the DRV8301 in low-power mode. But when enabling the DRV8301 from low-power mode by EN_GATE pin to high…
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: DRV8301 We are working on DRV8301-69M-KIT and using 1KW BLDC/ PMSM for all our development work. We use the same motor on desk as well mounting it on vehicle.
This is just for safety we used…
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: INSTASPINUNIVERSALGUI , MOTORWARE When working in Advanced: Field control & modulation section of GUI, SVM modulation was set to Quasi Sinusoidal by default but in user.h file USER_MAX_VS_MAG_PU…
Other Parts Discussed in Thread: DRV8301-69M-KIT Hi. I would like to explore using the DRV8301-69M-KIT to sinunsoidally drive a motor, but does the motor not have to also have a matching winding structure? I am interested in small motors for UAVs, can…
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: C2000WARE Hello TI,
We are working on 28069F MCU, we compiled the ECAN example code (Example_2806xECanBack2Back) from C2000Ware. Program build with no error but I'm facing a Warning with…
Part Number: DRV8301-69M-KIT I have a need to position the shaft to a specific position and put a small force to hold it there. Is there a way I can turn on a fixed current through the motor windings to hold that position?
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: MOTORWARE Tool/software: Code Composer Studio I have a few questions about DRV8301-69M-KIT board, Could you help on them?
1. Is it possible to directly use the GUI to read the motor parameters…
Part Number: DRV8312-69M-KIT
Hi Team,
I would like to buy DRV8312-69M-KIT for sensorless FOC.
I would like to know about the below details before proceeding further...
1. Does this kit include a PMSM motor?
2. The model number of the motor available…