Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: CONTROLSUITE Dear TI team
We are considering creating an evaluation environment incorporating this kit.
Can I please get a 3D (step file) or a mechanical drawing (DXF) of the KIT
…
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: DRV8301 , CONTROLSUITE Hi there
We have designed our own surface mounted PMSM motor, and trying to drive it with the DRV8301-69M-KIT. We have followed the PM sensorless field orientated control…
Part Number: DRV8301-69M-KIT Dear Yanming Luo: I have just noticed that there is a discussion in the forum that braking can be achieved by opening and closing the upper and lower sides. If the motor inductance is large, it will generate current spikes…
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: BOOSTXL-DRV8301 , DRV8301 , TMS320F28069M Is this a DSP evaluation board capable of controlling dc, bldc and step motors?
Is it possible to control the motor only with the motor drive expansion…
Part Number: LVSERVOMTR Other Parts Discussed in Thread: DRV8301-69M-KIT Hello,
i got the DRV8301-69M-KIT and LVSERVOMTR motor (verified to be Teknic_M2310PLN04K).
i redid lab 1b and 5e to make sure the wire connection and system ran correctly.
…
Part Number: DRV8301-69M-KIT I am having exactly the same problem as the other user in Lab11e.
The motor runs forward only if I input negative value in gMotorVars.SpeedRef_krpm and only runs at maximum RPM without caring for the value I have put in…
Part Number: DRV8301-69M-KIT Hi Team,
Good day. I am posting this inquiry on behalf or the customer.
"I already purchased a 69m kit for foc control of a brushless dc motor, but I wonder with some modifications in the hardware of the MISO CONTROL CARD…
Part Number: DRV8301-69M-KIT The flying start feature is used to start a rotating motor, as quickly as possible and resume normal operation with a minimal impact on load or speed. Similarly, In Torque Mode to start a rotating motor flying start is required…
Part Number: DRV8301-69M-KIT Hi Yanming:
Since the problem of offline operation was solved last time, the program debugging has been very smooth.
Until recently, when I wanted to test the program encryption, I found that once the project was encrypted…
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: MOTORWARE Dear team:
When my client uses the routine lab5c in motorware to perform the inertia identification test, the inertia identification state will jump back and forth between "ST_VEL_ID_INIT…