Part Number: DRV8301 Other Parts Discussed in Thread: DRV8323 Tool/software: Hi experts,
my customer is using the DRV8301-HC-C2-KIT in his test setup for motor control and quick prototyping to setup the verification setup.
Unfortunately the DRV8301…
Part Number: DRV8301-69M-KIT Hi TI team,
We developed our know controller board and driver board based on DRV8301-69M with 28069F/M MCU. We did integrity verification of the board and all where proper.
But one of the voltage offset (ADC- Vhb2 ) was…
Part Number: DRV8301-69M-KIT Hi TI team,
We are using torque loop in the BLDC mode to run the motor. But In the current loop they are tuning the Speed loop also, what is the need of tuning the Speed loop in current mode. When entering or exiting from…
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: CONTROLSUITE Dear TI team,
We are using DD motor which has two hall sensor. Can you provide the chart for running the BLDC control with 2 hall sensor input.
Regards
Part Number: DRV8301-69M-KIT
Hi TI,
We are using a motor of 2KW(48V) which can go up to 4000rpm. But when we set the speed ref to 2000rpm motor is not able to spin more than 1600rpm. We have increased the saturation limit of PI (speed and current…
Part Number: DRV8301-69M-KIT Hi sir,
I have the DRV8301-69m Kit. and I have three questions on this EVM.
can you help me to clarify them?
1) ADC data is obtained from 0 to 4095, what is the corresponding current value? I'm not sure, but it seems…
Part Number: DRV8301-69M-KIT Tool/software: Code Composer Studio Hi, when motor is coupled with load, motor starts to struggle in the initial pickup(acceleration), once the motor attains the acceleration its starts to move smoothy.Is there any parameter…
Part Number: DRV8301-69M-KIT Hi TI team,
For 28069F/M MCU TI suggest XDS110 and XDS200 debug probe.
When we see the compatible devices for XDS110 we could not find 28069F/M, but it is available in XDS200.
Kindly clarify which JTAG debug probe should…
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: MOTORWARE Hardware :
Invertor : DRV8301-69M kit based invertor with proper thermal/ heat sink design
MCU : F28069M controller
Software : Motorware / Torque control
We have customer…
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: MOTORWARE Hi all:
I have a very simple question, that is, how to make labs routines in motorware run in flash(without CCS connected, or called standalone mode?) and drive the motor to rotate…