Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: DRV8301 Tool/software: Code Composer Studio Hi
I am working on the TI DRV8301 for project lab5a. but i have question on what following code does
CTRL_getFlag_enableDcBusComp ()
inline…
Part Number: DRV8301-69M-KIT Hello TI,
We are working on the CAN protocol for 28069F MCU which supports the CAN-A module. But we need a secondary (external) CAN node to emulate the function of CAN-B. Kindly suggest some open-source/free USB-bus-based…
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: DRV8301 Hello TI team,
Whenever we update the drv setting (in drv setup function() ) we are not able to see the updated value in the watch window. So we increased the waiting time of drv…
Part Number: DRV8301-69M-KIT I am using the DRV8301-69M to drive a BLDC motor and have it working fine for generating the desired power output etc. However one thing I need is that after the motor has been ran I need for the motor to provide braking for…
Part Number: DRV8301-69M-KIT I am trying to utilize the eval board to both characterize a BLDC motor and to also run a test using the parameters. My basis is Lab5b. I have set up the serial port to be interrupt driven so that I can send commands to the…
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: MOTORWARE , DRV8301 Hello
I am trying to drive a motor at 48V using the DRV8301-69M-KIT.(No load 100 rpm)
Software is motorware Lab05b.
If Vdc is set to 44V or higher, the motor cannot…
Part Number: DRV8301-69M-KIT Earlier we posted questions on motor startup, thanks for the help. Finally we could start the vehicle/ motor successfully with BLDC mode during start up. We are using Lab 11e for our prototype testing.
Now the motor starts…
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: MOTORWARE Hi,
I have a Problem with the Labs. In the Lab 2 you have to estimate the Motorvalues (Code bellow)
#elif (USER_MOTOR == Q60) #define USER_MOTOR_TYPE MOTOR_Type_Pm #define USER_MOTOR_NUM_POLE_PAIRS…
Part Number: DRV8301-69M-KIT In startup is it necessary to use hall sensor to get more torque or can we achive this with FOC(sensorless) itself and hall for identify directions and position.
Thanks
Mofudrives
Part Number: DRV8301-69M-KIT Other Parts Discussed in Thread: DRV8301 Overcurrent trip is decided based on OC_ADJ_SET / MOSFET RDS(on). we are using a 750W 48V BLDC motor which has a rated current of 15A.
In our design,
MOSFET RDS = 0.0039ohm.
How…