Other Parts Discussed in Thread: DRV8302 Hello,
I tried to use com_trig module instead of InstaSPIN_BLDC module for the InstaSPIN_BLDC Software for DRV8302_HC_C2_Kit F28035 and when I start execution, the startup mode is working well and when the Ramp3DoneFlag…
Hello,
Now the project is built and the problem is that I have also to add these files and I do not why there are not any mention about them in the document:
DSP2803x_GlobalVariableDefs.c
DSP2803x_DefaultIsr.c
But I have another problem:
When…
a bit more clarification
The DRV8312 kit ships with a 24v power supply, so the GUI is set to throw faults if not in the +/- 10% range.
The DRV830x kit does not ship with a power supply, so the GUI is set to work across the operation range.
…
I am in a similar predicament. I have switched between non-real time and real time mode while the debugger is running, and each window is set to continuously refresh. Still no dice. However, my system is slightly different.
CCS version 5.2
DRV8302…
Hi everybody, and especially TI employees from Motor Control Dep.:
I am using DRV8302-HC-C2-Kit to control with high power motor (13.5 KW -HPD13.5-) and I calibrated the parameters for current control loop.
I made a model for this motor on MATLAB…
blipton said: The 'M' series piccolos have secure ROMs that support InstaSpin-MOTION (like the one found on the TMDSCNCD28054MISO control card),
Correct. The "M" devices also include InstaSPIN-FOC. The -MOTION just enables use of the SpinTAC Suite which…
Other Parts Discussed in Thread: INSTASPIN-BLDC , MOTORWARE , CONTROLSUITE , DRV8301 , TMS320F28027 , DRV8301-69M-KIT , RM48L952 Hello. This is my first time here. I have a little experience on DSP TMS320F28027 and I now plan to buy the DRV8301-HC-C2…
Other Parts Discussed in Thread: DRV8332 , DRV8302 I'm looking at using InstaSPIN-FOC (and maybe -MOTION) to control some very small outrunners which will become hub motors in a RC car. At the moment I'm playing with the DRV8312-69M-KIT. I'm already aware…
Dear Sir
I'm using the project GUI_project_InstaSPIN_BLDC of DRV830x-HC-C2-KIT_v104.
My motor is BLDC.
The MaxSpeed is 1000RPM. If I want more speed, like 2000RPM, how do I need to do?
Cause I modify the Gui.Ref to 1.2, the FaultFlag will set…