Ok..
First things first ... Many thanks for the help from the forum and your self Andrew with out your suggestions of a chip change I would have been a bit unsure.
As it stands today I've had a brushed motor spinning and quite high duty cycle ( @ 16Khz…
Part Number: DRV8302-HC-C2-KIT Hello Guys,
Good day.
In the DRV8302-HC-C2-KIT BOM file, a 140 mohms inductor rated at 1.5A were mentioned (DR74-330-R). However this Inductor is currently not available in the market. Is it okay to replace it with a 130 mOhms…
Part Number: DRV8302 Hi team,
Non-operational after power up, 1.5-K sawtooth on GVDD and GH_A, SH_A, the customer would like to know if this is this normal, or is it a kind of mode of operation?
Could you help check this? Thanks!
Best Regards,
Cherry …
Hi Benjamanas,
I will close this thread. Feel free to ask a related question by clicking the orange button at the top right of the window!
Thanks,
Matt
Part Number: DRV8302-HC-C2-KIT To whom it may concern,
I have three questions about the DRV8302-HC-C2-KIT current sensor. At first, when I saw the schematic, I wonder why 1 current shunt sensor(Ic) go through other circuit. On the other hand, 2 shunt…
Part Number: DRV8302-HC-C2-KIT Hi,
Good Day. I have a customer who is working with DRV8302-HC-C2-KIT. Please see below for his query about the DRV8302-HC-C2-KIT. Thank you very much.
Regarding the position manager feature of DRV8302 control kit board. …
Part Number: DRV8302-HC-C2-KIT
To whom it may concern
In DRV8302-C2-kit allocation and F28035 mux map, the hall inputs connect the GPIO40~42. And that ports have no eCAP in F28035. eCAP ports are GPIO 5, 19 ,24. That ports are allocated other things…
Part Number: DRV8302 Hi Team,
When an external 9v power supply is connected, the GVDD output is only about 6v.
When an external 20v power supply is connected, the GVDD output further drops to 2v.
The output of AVDD and DVDD is normal. But GVDD output…
Part Number: DRV8302
Dear Team,
We are using DRV8302 driver and our own controller, developing a 250w hub motor controller,
Hall sensor-based 6step commutation methods are used. initially, motor spin fine but some time fault occurs, here enclose the…