Hi Takashi,
Please click the resolve button to let us know if this issue has been resolved. Closing the thread for now. For further questions feel free to reopen the thread.
Best,
~Alicia
Part Number: DRV8305-Q1 Other Parts Discussed in Thread: DRV8305 Hello All, I am trying to simulate a motor driver in MATLAB Simscape and want to add the DRV8305 model to my project. I have attempted importing using the SPICE model listed under the link…
Part Number: DRV8305 Hi,
I have measured the back emf waveform between two motor terminals (phases) and it looks like so:
So I have 9V peak-peak (4.5V Amplitude).
It is sine, but in D-Q reference frame it will be constant DC waveform (at a specific speed…
Hi Cherry,
Cherry Zhou said: Hi Akshay and Brian,
Akshay Rajeev Menon said: Based on the schematic I believe this is a sensorless FOC correct?
Yes, correct.
For a sensorless motor, the driver needs to find the initial rotor position by either doing the Align…
Part Number: DRV8305 Helllo,
I want to add current sense filtering to DRV8305N and have the following questions:
1. Should I add filters both at the input and the output for the DRV8305 like in the below picture or maybe only at input or only output? …
Part Number: DRV8305 Other Parts Discussed in Thread: TMS320F28379D Hello,
My motor has 21V DC Link Voltage from battery.
I want to run it at 4000rpm.
I checked my motor the back EMF waveform rotating it from external and measuring motor phase voltages…
Part Number: 2MTR-DYNO I checked the motor PN, it is Teknic M-2310P-LN-04K, but I can't find the PIN definitions in TI, Can someone share me the official PIN definition and the motor parameters? Thanks.
Kan
Part Number: TMS320F28027F Other Parts Discussed in Thread: DRV8305 Hello
Greetings of the day!!!
I am using F28027F + DRV8305 for driving BLDC motor. I am using projlab05b.c. In projlab05b.c i have written follwing code
float A_RPM=5.0;count++; if(count…