Part Number: TMS320F28027F Other Parts Discussed in Thread: DRV8305 Hello
Greetings of the day!!!
I am using F28027F + DRV8305 for driving BLDC motor. I am using projlab05b.c. In projlab05b.c i have written follwing code
float A_RPM=5.0;count++; if(count…
Part Number: 2MTR-DYNO I checked the motor PN, it is Teknic M-2310P-LN-04K, but I can't find the PIN definitions in TI, Can someone share me the official PIN definition and the motor parameters? Thanks.
Kan
Part Number: INSTASPIN-BLDC Other Parts Discussed in Thread: TIDA-00643 , DRV8305 Hello
I am working on TIDA-00643 reference design.
I wanted to check what are the SPI configuration in projlab5b.
How and where to locate the commands in project?
Part Number: LAUNCHXL-F28379D Other Parts Discussed in Thread: 2MTR-DYNO , , BOOSTXL-DRV8305EVM , DRV8305 , SFRA , CONTROLSUITE , C2000WARE Hello, i have a similar problem to this thread.
I have the same set: LAUNCHXL-F28379D, two BOOSTXL-DRV8305EVM's, and…
Part Number: DRV8305-Q1 hi expert
For ULVO function in datasheet, i have two questions
Q1: How can i understand the parameter of PVDD falling and PVDD rising?
Let us assume PVDD is 10V now, when PVDD is rising to 42.5V(10V+32.5V( shown in datasheet )) because…
Hello,
Closing thread for now - but as mentioned above, please feel free to click the button for 'ask a related question' and reference this e2e thread to continue the conversation. Thanks!
Best Regards, Andrew
Part Number: DRV8305 I have a 3phase BLDC motor driver using DRV8305. During deceleration, I'm considering closing only the low side switches (all 3 simultaneously) to perform eddy current braking while using low side shunts to monitor the current so…
Hey Alessio,
Please click the resolve button to let us know if this issue has been resolved.
Closing the thread for now. For further questions feel free to reopen the thread.
Best,
Akshay
Part Number: DRV8305-Q1 Other Parts Discussed in Thread: DRV8305 Hello,
we are using the DRV8305NQPHPQ1 as the gate driver for our BLDC motor control board and are experiencing a jump in the the total current to the board from 70 mA to 390 mA when the…