Part Number: DRV8305-Q1EVM Tool/software: Dear TI experts,
Can I know the purpose of D11, D12, D13 schottky diodes?
I attach the one of schematic in DRV8305-Q1EVM.
Best regards,
Chase
Part Number: DRV8305-Q1EVM Other Parts Discussed in Thread: DRV8305 , DRV3255-Q1 , DRV8363-Q1 , DRV8363-Q1EVM Tool/software: I am running a DRV8305-Q1EVM board with a high speed motor with a 34V power supply. I also use the InstaSPIN_UNIVERSAL software…
Part Number: DRV8305-Q1EVM Other Parts Discussed in Thread: DRV8305 Tool/software: Hi TI
I use drv8305 and drv8714 in my design,and connected two ICs use a SPI bus.
When I set drv8305 go sleep mode,I can not read DRV8714's register(SPI bus go abnormal…
Part Number: DRV8305-Q1EVM Other Parts Discussed in Thread: DRV8305-Q1 , MOTORWARE , CCSTUDIO Hi,
We are using DRV8305-Q1 EVM to run a BLDC motor. I have used the following steps
1) J3 jumper is changed to USB and loaded the code using micro-USB and…
Part Number: DRV8305-Q1EVM Other Parts Discussed in Thread: TMS320F28027F Customer would like to use similar design as DRV8305-Q1EVM did for their water pump design, with sensorless control scheme. They wanted to remove BEMF sensing circuits. However…
Part Number: DRV8305-Q1EVM Other Parts Discussed in Thread: MOTORWARE Hi,
We have started the InstaSpin FOC with a BLDC motor. Now once we put the speed reference as 1500 RPM, the motor reaches to 1325 rpm and remains on that speed, even after giving…
Part Number: DRV8305-Q1EVM Other Parts Discussed in Thread: DRV8305 Hi Team,
Using F28069M+drv8305 for m otor control and the control algorithm being used is motor ware's InstaSPIN-FOC.
At 900 control frequency per second, if a fixed control current…
Part Number: DRV8305-Q1EVM Other Parts Discussed in Thread: DRV8305 , C2000WARE , C2000WARE-MOTORCONTROL-SDK I need to write code for the LaunchPad XL F28379D and DRV8305 that will be used to detect the correct angle of an encoder using hall sensor signals…
Part Number: DRV8305-Q1EVM Other Parts Discussed in Thread: MOTORWARE Hi,
use DRV8305-Q1EVM module Board and I use proj_Lab02b software. This software includes EST Module. When motor is started, this EST module estimates motor parameter. Then, control…