Part Number: DRV8306 Other Parts Discussed in Thread: MCT8316Z Hello,
I have designed a schematic using drv8306 to drive a motor with 24V, 5A.
please help to review the schematic.
Thanks.
Chester
drv8603_Schematic1_2026-05-24.pdf
Part Number: DRV8306 The DRV8306 datasheet says that absolute max value for HPA, HPB, HPC etc. is DVDD. It also says that exceeding these values may cause permanent damage, etc.
The datasheet then says that DVDD min is 2.9, typ is 3.3, and max is 3…
Part Number: DRV8306 Tool/software: Hi,
I am presently building a 28V 60W BLDC drive using DRV8306. The basic functionality tests viz., slow start, run at full speed, etc. with the 60W motor connected to a fan load using DRV8306 was initially validated…
Part Number: DRV8306 Tool/software: Hello,
Need help.
We use DRV8306 to drive a motor, but we must need to use external GATE-DRIVER (BOOTSTRAP) to drive MOSFET for HIGHSIDE and LOWSIDE. Therefore, we only need to GHA (PIN5), GHB (PIN11), GHC (PIN12…
Part Number: DRV8306 Tool/software: Hello TI community,
we are developing a BLDC driver PCB using DRV8306. The motor shall run at full speed or stand still by applying HIGH or LOW to the PWM pin. This would allow for a very simple interfacing method…
Part Number: DRV8306 Other Parts Discussed in Thread: UCC27710 Tool/software: Hello team ,
Please suggest me a suitable solution for driving the motor with the below details. Below mentioned Motor is used for Solar water pump
Motor Power 3HP
Motor…
Part Number: DRV8306 Tool/software: Hello TI Community,
I'm currently working on a BLDC motor control project using the DRV8306. The motor has hall sensors for feedback.
However, I'm facing some issues:
The output waveform is distorted; it's…
Part Number: DRV8306 Other Parts Discussed in Thread: MCT8315Z Tool/software: Hello,
For my application 1kW 24V motor i need sensored solution with integrated control.
Is DRV8306 a good choice? It has rather small gate drive strength (but probably…
Part Number: DRV8306
Hi, experts.
I am encountering issues with the Motor Driver DRV8306 and Ti Mosfet CSD88584.
I chose this mosfet after observing it on TI's EVM Board, which utilized the DRV8306 and CSD88584 Mosfet.
My system comprises an ST…
Part Number: DRV8306 Tool/software: 1780.BLDC_DRIVER.pdf
Hi, I am making a custom BLDC motor driver, here is the schematic. The mosfets I'm using is IRFR3708TRPBF. The start up sequence is driver -> controller. Controller starting with direction and…