Hi Asley,
Thank you for your comment!
If you have any questions related to this topic please click the orange "Ask a related question" button at the top left of your screen.
Regards,
Joshua
Part Number: DRV8306 Other Parts Discussed in Thread: INA236 hello.
I used a translator.
I am driving a BLDC motor with the DRV8306 motor driver.
I am reading data with ADC by connecting a differential amplifier to both ends of Rsense. I found something…
Part Number: DRV8306 Other Parts Discussed in Thread: CSD88584Q5DC Hi,
The customer manufactured a board with DRV8306 & CSD88584Q5DC applied.
BLDC Motor is not operated during board verification, so it is necessary to review for design and setup errors…
Part Number: DRV8306 This question is related to DRV8306: DVDD [PIN 26] of DRV8306HRSMT is showing 4.2 to 4.8V.
Despite of all attempts, when we were unable to solve the issue - we suspected random issue & discarded the board.
And created a fresh version…
Part Number: DRV8306 Hi Team,
The enable signal is high level, the PWM frequency is 10KHz, and the duty cycle is 50%. But the high side of the three half bridges is 0V, and the low side is 10V. The 3 Hall signals of the motor have normal input. Here is the…
Hi on,
For DRV8306, you can try configuring the VDS OCP threshold by changing the resistor as specified here in the datasheet:
Keep in mind that this measures VDS of the FET, so you will need to do the calculation of your peak current * Rdson to find…
Part Number: DRV8306 Other Parts Discussed in Thread: LM5113 Does this driver support the use of GanFet's or is it only designed for the use of MosFets?
Part Number: DRV8306 Other Parts Discussed in Thread: DRV8353 Hello,
Is it possible to drive motor by a separate voltage than driver, i.e. 24V for driver and 60V for Mosfet/motor?
And use voltage divider for Vdrain? I understand the measure of the current…
Part Number: DRV8306 MC33035DW.PDF
DRV8306 38-V Brushless DC Motor Controller datasheet.pdf
Dear Sir,
I need to provide an analysis of the Motor Controllers performance difference, I would like to ask DRV8306 & MC33035DW which key point of the driving…
Part Number: DRV8306 Hi team,
According to the manual, FGOUT is used to measure speed, but it does not specify how many pulses a FGOUT can have in one turn. How to test the speed with FGOUT? Thanks.
Best Regards,
Cherry