Part Number: DRV8306 Hi Team,
The enable signal is high level, the PWM frequency is 10KHz, and the duty cycle is 50%. But the high side of the three half bridges is 0V, and the low side is 10V. The 3 Hall signals of the motor have normal input. Here…
Part Number: DRV8306 Other Parts Discussed in Thread: CSD88584Q5DC Hi,
The customer manufactured a board with DRV8306 & CSD88584Q5DC applied.
BLDC Motor is not operated during board verification, so it is necessary to review for design and setup errors…
Part Number: DRV8306 Other Parts Discussed in Thread: LM5113 Does this driver support the use of GanFet's or is it only designed for the use of MosFets?
Part Number: DRV8306 Hi team,
Here's an issue from the customer may need your help:
How to connect the three Hall sensors of DRV8306? The customer chose a three-pin hall sensor, how should they connect it? Or is the three-pin Hall sensor not acceptable…
Part Number: DRV8306 This question is related to DRV8306: DVDD [PIN 26] of DRV8306HRSMT is showing 4.2 to 4.8V.
Despite of all attempts, when we were unable to solve the issue - we suspected random issue & discarded the board.
And created a fresh…
Part Number: DRV8306 We have tested DRV8306 with two lots. We found the phase commutation logic inconsistent. Please refer attachment.
The phase connection U, V & W does not work in New lot (V W & U works).
Please justify the above. All our circuitry…
Part Number: DRV8306 Other Parts Discussed in Thread: INA236 hello.
I used a translator.
I am driving a BLDC motor with the DRV8306 motor driver.
I am reading data with ADC by connecting a differential amplifier to both ends of Rsense. I found something…
Part Number: DRV8306 We are using DRV8306 inorder to drive the motor. Motor is having no load speed of 24K Rpm and no load current is 200mA at 24V. Attached the datasheet of motor & schematics. We had increased the speed by increasing the dutycycle of…
Part Number: DRV8306 Hi team,
According to the manual, FGOUT is used to measure speed, but it does not specify how many pulses a FGOUT can have in one turn. How to test the speed with FGOUT? Thanks.
Best Regards,
Cherry