Part Number: DRV8306 Other Parts Discussed in Thread: DRV8353 Hello,
Is it possible to drive motor by a separate voltage than driver, i.e. 24V for driver and 60V for Mosfet/motor?
And use voltage divider for Vdrain? I understand the measure of the…
Part Number: DRV8306 Other Parts Discussed in Thread: DRV10987 Hi,
Is there any MCU software for DRV8306? I need PI control software for DRV8306 using MSP or C2000.
Best regards, Sasaki
Part Number: DRV8306 Other Parts Discussed in Thread: CSD88584Q5DC , CSD87333Q3D
I used a translator. Please excuse me.
Hi. I am inquiring about the DRV8306 motor driver.
I attached the data sheet and circuit diagram of the BLDC motor that I…
Part Number: DRV8306 Hi Team,
DRV8306 architecture Hall must be independently connected to positive and negative. customer motor has a signal output for A&B&C Hall, and a Ground and VDD. Can the logic pin be changed to 5V?
Part Number: DRV8306 HI TI Expert,
We now use DRV8306 to drive a BLDC. below is motor parameter
According system demand, We need the motor running between 50-700ms per every second.
below is a typical application, that's what we want. ch1 pwm…
Part Number: DRV8306 Other Parts Discussed in Thread: LM5121 , We are using the IC DRV8306 & the boost LM5121. Boost section we loaded upto 10A with electronic load. Also DRV we run upto 10A with the motor. Both are working independently. We had tried…
Part Number: DRV8306 Other Parts Discussed in Thread: DRV8308 , , DRV8307 Hi
In DRV8308 datasheet 7.3.13.2 VM Overvoltage (VMOV) talk about "energy from the mechanical system can be forced back into the VM power supply. This can result in the VM power…
Part Number: DRV8306 Hi,
Please help me with a review of the below schematic for the DRV8306. Following are some of the changes that I have done already on board but then looking to see if there is something more that needs to be done.
C77 is updated…
Part Number: DRV8306 As per last reply, we have checked the VM & DVDD nets on scope.
We find out very strange behaviour of DVDD pin.
Our observation as below
#1 : At start up VM rise pattern looks normal. And then the voltage on the VM appears as…
Part Number: DRV8306 Hi team,
Customer currently stops motor's rotating by using the nBRAKE pin (H to L). But the motor we are using has very low friction, so it takes a long time to stop.
Is there any way to make this brake faster by DRV8306 settings…