Part Number: DRV8308EVM Other Parts Discussed in Thread: DRV8306EVM , DRV8306
Hi,
We're planning to use DRV8306EVM and DRV8308EVM for evaluation of 3-phase BLDC motor.
We're using DRV8306EVM (or DRV8308EVM) to drive NEMA17, 3-phase BLDC motor. Motor…
Part Number: DRV8306EVM Other Parts Discussed in Thread: DRV8308 , DRV8306
Hi,
I'm using DRV8306-EVM to evaluate scroll compressor. I observed that there is significant SPEED drop (approx. 90 rpm) when there is small change in load. Hall Sensor: 102…
Part Number: DRV8306 Other Parts Discussed in Thread: MCT8329EVM , MCF8329EVM , , DRV8329 , DRV8323 Tool/software: Hello Team,
We have below evaluation board for BLDC motor testing. with this board we have tested BLDC motor in trapezoidal sensored mode…
Part Number: DRV8306EVM Other Parts Discussed in Thread: DRV8306
I am using the DRV8306EVM to drive a BLDC motor and seeing some unexpected current flow during one of the stages of commutation where both the high and low side FETs are turned off. In…
Part Number: DRV8306EVM Other Parts Discussed in Thread: DRV8306 , CSD88584Q5DC , CSD88599Q5DC
Hi
I design a circuit like DRV8306EVM board for drive a sensored BLDC motor with nominal voltage 24V and nominal current about 4A. My motors datasheet is available…
Part Number: DRV8306EVM Other Parts Discussed in Thread: DRV10987 Hello there. I want to ask you something. DRV8306EVM.
I have my sensorless motor. Can you run the sensorless motor with this product? I don't want to use the HPA, HNA, HPB, HNB ... pins.…
Hello Tomer,
Your calculations care correct, at 30 A the R29 shunt resistor on the DRV8306EVM would fail. The DRV8306EVM is limited to support a maximum of 16A due to the max current rating of the J5 connector ( 691101710002 ) used for VM. This limits the…
Hello Tomer,
Tomer Bruchiel said: I would like to understand how to calculate R_ISEN?
Your calculations are correct if you are attempting to determine a Rsense value for a Pulse-by-Pulse limit of 40A. On the DRV8306EVM the Pulse-by-Pulse current limit…
Part Number: DRV8306 We have built an integrated driver circuit based on the DRV8306EVM and need the formula to calculate the R29 value to control our output current.
Can anyone please share this formula?...it does not appear in TI documentation and is…
Hi Amol, Please evaluate the DRV8306EVM . It is a PWM controlled gate driver with sensored trapezoidal control and Hall sensor feedback. You could also look at using 1x PWM mode in the following devices/EVMs:
DRV832x BOOSTXL-DRV8320S BOOSTXL-DRV8320H BOOSTXL…